+1 500 000 products in offer

7000 packages per day

+300 000 clients from 150 countries

Quick Buy Favourites
Cart

Osmosis - definition

Osmosis is a physicochemical phenomenon involving the spontaneous, directional flow of a solvent - usually water - across a semi-permeable membrane separating two solutions of different concentrations of solute. The semi-permeable membrane allows the free transport of solvent molecules, but blocks the passage of most of the solute molecules, leading to an equalisation of chemical potentials between the two sides of the system. The direction of osmosis always leads from a less concentrated (hypotonic) solution towards a more concentrated (hypertonic) solution, increasing its volume and diluting its concentration.

The phenomenon of osmosis is crucial in cell biology, where it regulates the water balance of organisms and maintains homeostasis. Osmotic equilibrium affects the shape, tension and function of plant and animal cells, especially in relation to turgor pressure. From the point of view of thermodynamics, osmosis occurs to minimise the free energy of the system.

In chemical engineering and membrane technology, osmosis is used, among other things, in water filtration and purification processes such as reverse osmosis, in which an applied external pressure opposes the natural flow, allowing pure solvent to be obtained from highly contaminated solutions. Osmotic processes are also used in the food, pharmaceutical and energy industries, where precise control of membrane permeability and osmotic pressure gradients is critical to technological efficiency.

Transfer Multisort Elektronik (TME) is one of the world’s largest global distributors of electronic components, electrotechnical parts, workshop equipment, and industrial automation. The catalog includes over 1,500,000 products from 1,300 leading manufacturers. TME’s modern logistics centers in Łódź and Rzgów (Poland), with a combined area of over 40,000 m², ship nearly 6,000 packages daily to customers in more than 150 countries.

TME also invests in the development of knowledge and skills of young engineers and electronics enthusiasts through the TME Education project, and supports the tech community by organizing the TechMasterEvent series, promoting innovation and experience exchange.

READ ALSO