+1 500 000 products in offer

7000 packages per day

+300 000 clients from 150 countries

Quick Buy Favourites
Cart

PCMCIA - definition

The PCMCIA (Personal Computer Memory Card International Association) is an expansion card interface standard developed for mobile computers that defines both the physical design of the cards and the communication protocols between the card and the system. The technology was introduced in the early 1990s by an organisation of the same name for computer and peripheral equipment manufacturers. Its aim was to create a universal, compact solution to extend the functionality of mobile computers.

PCMCIA cards, also known as PC Cards, resembled flat credit cards in appearance and size, and were equipped with a 68-pin connector, allowing direct connection to a special slot in a laptop. The standard provided for three types of card, differing mainly in thickness, to support a variety of devices from flash memory and modems to network adapters, SCSI interfaces, disk controllers and I/O extensions.

PCMCIA technology was based on the ISA bus and later also PCI, offering automatic discovery and configuration mechanisms (Plug and Play), which greatly simplified hardware installation. As technology evolved and the demand for higher bandwidth, the standard evolved into CardBus, a 32-bit version of PCMCIA, electrically compatible with the PCI bus, and ExpressCard, based on PCI Express and USB.

PCMCIA has played an important role in the history of mobile computing development, enabling it to be flexibly adapted to different tasks without the need for external peripherals. Although it has been superseded in newer designs by more compact and faster solutions such as USB or integrated internal modules, for many years it has been the standard method of extending the capabilities of notebooks and mobile terminals.

Transfer Multisort Elektronik (TME) is one of the world’s largest global distributors of electronic components, electrotechnical parts, workshop equipment, and industrial automation. The catalog includes over 1,500,000 products from 1,300 leading manufacturers. TME’s modern logistics centers in Łódź and Rzgów (Poland), with a combined area of over 40,000 m², ship nearly 6,000 packages daily to customers in more than 150 countries.

TME also invests in the development of knowledge and skills of young engineers and electronics enthusiasts through the TME Education project, and supports the tech community by organizing the TechMasterEvent series, promoting innovation and experience exchange.

READ ALSO