+1 500 000 products in offer

7000 packages per day

+300 000 clients from 150 countries

Quick Buy Favourites
Cart

PMIC (Power Management Integrated Circuits) - definition

PMICs (Power Management Integrated Circuits) are integrated circuits used to manage the distribution and conversion of electrical power in electronic devices. Their purpose is to provide stable voltages and currents to various sections of an electronic system, while optimising power consumption and providing protection against overload, overheating and other undesirable operating conditions. PMICs are key components in modern mobile devices, computers, embedded systems and battery-powered applications.

The PMIC structure can include many functions, such as voltage converters (buck, boost, buck-boost), linear stabilisers (LDOs), voltage monitoring circuits, battery charge management, multiplexing of power sources, supervision of subsystem power-up sequences or power management in sleep and standby modes. The integration of these functions in a single chip reduces the number of components on the PCB, improves energy efficiency and simplifies the design of the power system.

PMICs are often designed to work with specific processors, microcontrollers or hardware platforms, taking into account their power voltage, start-up sequence and power profile requirements. Their configuration can be implemented through digital interfaces such as I²C, SPI or dedicated configuration pins, enabling real-time dynamic control of operating parameters. In this way, PMICs support adaptive power management functions, reducing power consumption according to the current needs of the application.

The use of PMICs is indispensable in designs where low power loss, high reliability and compact dimensions are required. In advanced systems such as smartphones, laptops, IoT devices or automotive systems, the PMIC acts as a central element controlling the power supply to all key components, directly influencing the performance, battery life and safety of the entire system.

Transfer Multisort Elektronik (TME) is one of the world’s largest global distributors of electronic components, electrotechnical parts, workshop equipment, and industrial automation. The catalog includes over 1,500,000 products from 1,300 leading manufacturers. TME’s modern logistics centers in Łódź and Rzgów (Poland), with a combined area of over 40,000 m², ship nearly 6,000 packages daily to customers in more than 150 countries.

TME also invests in the development of knowledge and skills of young engineers and electronics enthusiasts through the TME Education project, and supports the tech community by organizing the TechMasterEvent series, promoting innovation and experience exchange.

READ ALSO