+1 500 000 products in offer
7000 packages per day
+300 000 clients from 150 countries
Pneumatics is the technical field dealing with the use of compressed gas, most commonly air, to transfer and control energy in mechanical systems. It is based on the physical properties of gases such as elasticity, compressibility and the ability to store energy under pressure. Pneumatics is used in actuator drives, industrial automation systems, material handling systems, as well as medical devices and hand tools.
The basic components of pneumatic systems are compressors, which generate compressed air, and air preparation units including filters, dryers and pressure regulators to ensure the quality of the working medium. The energy carried by the compressed air is used to perform mechanical work through linear and rotary actuators, pneumatic drives or robotic grippers mechanisms.
Characteristic features of pneumatic systems are high dynamic performance, simplicity of design, safety of use and ease of maintenance. Pneumatics, on the other hand, has the disadvantage of relatively low energy efficiency due to unavoidable heat losses during compression and expansion of air. Modern pneumatic systems use advanced proportional and digital control technologies, integrating electrically controlled valves (solenoid valves) and condition diagnostic systems to enable precise motion control and increase the reliability of entire systems.
In engineering practice, Pneumatics co-exists with Hydraulics and Electrical Automation to form complex mechatronic systems, where the choice of operating medium depends on the application requirements for force, speed, precision and environmental conditions of the equipment.
Transfer Multisort Elektronik (TME) is one of the world’s largest global distributors of electronic components, electrotechnical parts, workshop equipment, and industrial automation. The catalog includes over 1,500,000 products from 1,300 leading manufacturers. TME’s modern logistics centers in Łódź and Rzgów (Poland), with a combined area of over 40,000 m², ship nearly 6,000 packages daily to customers in more than 150 countries.
TME also invests in the development of knowledge and skills of young engineers and electronics enthusiasts through the TME Education project, and supports the tech community by organizing the TechMasterEvent series, promoting innovation and experience exchange.