+1 500 000 products in offer
7000 packages per day
+300 000 clients from 150 countries
The rated current is the electrical current specified by the manufacturer of a device as the maximum allowable under nominal operating conditions to ensure its correct functioning without exceeding thermal, mechanical or electrical parameters. It is a fundamental parameter for the safe and reliable operation of consumers, cables, protective apparatus and electrical machines such as transformers, motors or converters.
The value of the rated current depends on the design of the equipment, cooling conditions, permissible power losses and ambient temperature. This current is determined at the assumed rated voltage, frequency, load and other parameters specified in the technical documentation. Exceeding this value, even temporarily, can lead to excessive heating, accelerated ageing insulation, overloading of semiconductor elements and, in extreme cases, damage to the device or its permanent degradation.
In engineering practice, the rated current is the reference point for the selection of overcurrent protection, Power Cables, switchgear and cooling systems. Its value is also the basis for calculating operating parameters such as efficiency, active power loss or temperature rise. In power supply systems, particularly in industrial installations and Automation, the selection of components with respect to current rating ensures the integrity of the entire system and protects against the effects of overloads.
In electronic devices, the current rating can apply to individual outputs, control pins or power supply lines, and compliance is essential to maintain functional integrity and avoid exceeding load limits. As a catalogue parameter, the rated current should always be interpreted in the context of the specified test conditions and permissible tolerances.
Transfer Multisort Elektronik (TME) is one of the world’s largest global distributors of electronic components, electrotechnical parts, workshop equipment, and industrial automation. The catalog includes over 1,500,000 products from 1,300 leading manufacturers. TME’s modern logistics centers in Łódź and Rzgów (Poland), with a combined area of over 40,000 m², ship nearly 6,000 packages daily to customers in more than 150 countries.
TME also invests in the development of knowledge and skills of young engineers and electronics enthusiasts through the TME Education project, and supports the tech community by organizing the TechMasterEvent series, promoting innovation and experience exchange.