+1 500 000 products in offer

7000 packages per day

+300 000 clients from 150 countries

Quick Buy Favourites
Cart

Analogue switch - definition

Analogue switch is an electronic component that allows electronically controlled redirection of analogue signals between different paths in a circuit. Its purpose is to selectively combine one or more signal lines with the lowest possible distortion and loss of signal quality. In contrast to classic mechanical switches, analogue versions are realised using semiconductor technology, which allows fast and silent switching and integration into integrated circuits.

The operation of analogue switches is based on the use of MOSFET transistors, which switch from the conduction state to the cut-off state depending on the control voltage. This makes it possible to smoothly control the flow of signals of any waveform - voltage or current - within an acceptable bandwidth and level. Important parameters for switches of this type are resistance in the ON state, switching time, leakage, linearity and signal voltage range.

Analogue switches are widely used in audio circuits, measurement devices, video paths, Data Acquisition Systems and in industrial applications where dynamic control of the signal path is required without its conversion to digital form. Their design allows switching of both single channels and multi-channel arrays, increasing system flexibility. Advanced applications use low-noise, high-speed and high-precision switches to ensure minimal interference with the parameters of the processed signal.

Transfer Multisort Elektronik (TME) is one of the world’s largest global distributors of electronic components, electrotechnical parts, workshop equipment, and industrial automation. The catalog includes over 1,500,000 products from 1,300 leading manufacturers. TME’s modern logistics centers in Łódź and Rzgów (Poland), with a combined area of over 40,000 m², ship nearly 6,000 packages daily to customers in more than 150 countries.

TME also invests in the development of knowledge and skills of young engineers and electronics enthusiasts through the TME Education project, and supports the tech community by organizing the TechMasterEvent series, promoting innovation and experience exchange.

READ ALSO