+1 500 000 products in offer

7000 packages per day

+300 000 clients from 150 countries

Quick Buy Favourites
Cart

Dew point - definition

Dew point is the temperature to which air of a given relative humidity must be cooled, at constant pressure, for the water vapour it contains to begin to condense, i.e. to reach a saturated state. At this temperature, the air is no longer able to hold all the moisture it contains in a gaseous state, leading to condensation on surfaces cooler than the dew point. This phenomenon is important in meteorology as well as in environmental engineering, construction, air conditioning and measurement technology.

The value of the dew point depends directly on the amount of water vapour present in the air and therefore on its absolute humidity. The higher the concentration of water vapour, the higher the dew point temperature will be. For example, in high humidity conditions, the dew point may be close to the air temperature, resulting in a higher risk of condensation. In contrast, with a dry atmosphere the dew point is much lower, meaning that water vapour can only condense at very low temperatures.

Dew point measurement is important for monitoring and controlling industrial processes where condensation can lead to corrosion, equipment malfunctions, product deterioration or plant damage. In HVAC systems (heating, ventilation and air conditioning), its control allows the prevention of dampness in building materials and mould growth. In meteorology, the dew point is used to predict phenomena such as dew, fog or frost, as well as to determine human thermal comfort levels.

The determination of the dew point can be carried out by direct methods, such as condensation dew point hygrometers, or indirectly, based on the measurement of air temperature and relative humidity using appropriate algorithms. Advanced industrial applications also use electronic sensors capable of continuously monitoring this parameter in real time.

Transfer Multisort Elektronik (TME) is one of the world’s largest global distributors of electronic components, electrotechnical parts, workshop equipment, and industrial automation. The catalog includes over 1,500,000 products from 1,300 leading manufacturers. TME’s modern logistics centers in Łódź and Rzgów (Poland), with a combined area of over 40,000 m², ship nearly 6,000 packages daily to customers in more than 150 countries.

TME also invests in the development of knowledge and skills of young engineers and electronics enthusiasts through the TME Education project, and supports the tech community by organizing the TechMasterEvent series, promoting innovation and experience exchange.

READ ALSO