+1 500 000 products in offer

7000 packages per day

+300 000 clients from 150 countries

Quick Buy Favourites
Cart

Pyranometer - definition

The Pyranometer is a precision measuring instrument used to record the total solar radiation reaching the horizontal surface from the sky hemisphere. It includes both direct radiation and radiation scattered in the atmosphere. Pyranometers are used in meteorology, solar energy, precision agriculture and climate research, where precise measurement of irradiance is crucial for assessing the energy balance and efficiency of photovoltaic systems.

The pyranometer's operating principle is based on the thermoelectric effect - solar radiation incident on the sensor's black-coated surface causes it to heat up, and the temperature difference between the absorbing surface and the reference body generates a voltage proportional to the intensity of the radiation. This signal can be recorded and processed by the measurement system, allowing a value to be obtained, usually expressed in watts per square metre (W/m²).

To ensure accuracy and repeatability of measurements, pyranometers are equipped with domes made of materials that transmit radiation over a wide range of wavelengths, from ultraviolet to near infrared . The dome protects the sensor from the effects of wind, rain and dirt, while minimising errors due to reflections and thermal losses. Professional applications also use calibration systems, self-cleaning mechanisms and dome heating, allowing long-term reliable operation in variable environmental conditions.

The accuracy of pyranometric measurements is crucial in the prediction of energy production from solar installations, in climatic analysis and in the validation of numerical models describing energy flow in atmospheric systems. Depending on the class of instrument (e.g. class ISO), pyranometers can be used for both reference measurements and operational tasks in the field.

Transfer Multisort Elektronik (TME) is one of the world’s largest global distributors of electronic components, electrotechnical parts, workshop equipment, and industrial automation. The catalog includes over 1,500,000 products from 1,300 leading manufacturers. TME’s modern logistics centers in Łódź and Rzgów (Poland), with a combined area of over 40,000 m², ship nearly 6,000 packages daily to customers in more than 150 countries.

TME also invests in the development of knowledge and skills of young engineers and electronics enthusiasts through the TME Education project, and supports the tech community by organizing the TechMasterEvent series, promoting innovation and experience exchange.

READ ALSO