+1 500 000 products in offer
7000 packages per day
+300 000 clients from 150 countries
Reluctance is a physical quantity describing the resistance that a given magnetic circuit places on the flow of magnetic flux. It is analogous to resistance in electrical circuits, but refers to phenomena occurring in a magnetic field. Reluctance depends on the geometry of the magnetic circuit and the properties of the materials of which it is constructed, primarily the length of the magnetic path, the cross-sectional area and the magnetic permeability of the medium.
Mathematically, reluctance is defined as the ratio of magnetomotive force (MMF) to magnetic flux. In the SI system of units is expressed in ampere per weber (A/Wb). It increases with the length of the flux path and decreases with increasing cross-sectional area or the use of material with higher magnetic permeability. Vacuum and air, which have a very low permeability, have a high reluctance, while ferromagnetic materials such as steel or iron have a much lower reluctance.
Reluctance plays a key role in the design of transformers, Coils, motors and electromagnetic devices, where proper guidance of magnetic fluxes allows high energy efficiency to be achieved. Technical practice also takes into account the non-linearity of reluctance, resulting from the saturation of magnetic materials and the presence of air gaps in cores. In magnetic circuits, as in electrical circuits, analogies to Ohm's law are used, allowing flux flow to be modelled using simplified circuit equations.
Understanding and controlling reluctance allows magnetic circuits to be optimised for losses, inductance and field distribution, which is important both in power devices and in sensors or actuators for automation systems .
Transfer Multisort Elektronik (TME) is one of the world’s largest global distributors of electronic components, electrotechnical parts, workshop equipment, and industrial automation. The catalog includes over 1,500,000 products from 1,300 leading manufacturers. TME’s modern logistics centers in Łódź and Rzgów (Poland), with a combined area of over 40,000 m², ship nearly 6,000 packages daily to customers in more than 150 countries.
TME also invests in the development of knowledge and skills of young engineers and electronics enthusiasts through the TME Education project, and supports the tech community by organizing the TechMasterEvent series, promoting innovation and experience exchange.