+1 500 000 products in offer

7000 packages per day

+300 000 clients from 150 countries

Quick Buy Favourites
Cart

Reostat - definition

The rheostat is an adjustable resistor with a variable resistance value, used in electrical and electronic systems to control current and regulate voltage in direct current (DC) and alternating current (AC) circuits. Its operation is based on Ohm's principle, according to which a change in resistance results in a modification of the current flow in the circuit, which is used in load control, parameter control of electric motors and in laboratory systems requiring precise adjustment of electrical values.

The design of the rheostat includes a conductive resistive element made of materials with high thermal stability and low temperature coefficient, such as nickel-chromium alloys, manganese or Constantan. A slide or slider mechanically moved across the surface of the resistive path changes the effective circuit length, which affects the electrical resistance value at a given control point. Depending on the design, rheostats can be in wire, film or liquid form, where the conducting medium is electrolyte with an adjustable conduction path length.

High-power systems use air- or liquid-cooled rheostats to dissipate the heat generated by the Joule effect and maintain stable operating conditions. Control mechanisms can use either manual knob control or remote mechanical or electronic control systems for automated applications.

Rheostats are a key component in applications requiring smooth current control, such as brightness control of lighting, speed control of DC motors and compensation for changes in load resistance in metering systems. In power systems, they are used as start-up resistors in high-power motors and as damping elements in dynamic braking systems. In modern applications, their function is increasingly being taken over by solid-state controllers such as PWM controllers or transistor power controllers, but rheostats are still used where a simple, reliable and mechanically robust control solution is required.

Transfer Multisort Elektronik (TME) is one of the world’s largest global distributors of electronic components, electrotechnical parts, workshop equipment, and industrial automation. The catalog includes over 1,500,000 products from 1,300 leading manufacturers. TME’s modern logistics centers in Łódź and Rzgów (Poland), with a combined area of over 40,000 m², ship nearly 6,000 packages daily to customers in more than 150 countries.

TME also invests in the development of knowledge and skills of young engineers and electronics enthusiasts through the TME Education project, and supports the tech community by organizing the TechMasterEvent series, promoting innovation and experience exchange.

READ ALSO