+1 500 000 products in offer
6000 packages per day
+300 000 clients from 150 countries
Resublimation, also known as desublimation, is a phase transformation involving the direct transition of a substance from the gaseous to the solid state, bypassing the liquid phase. This process occurs under conditions of sufficiently reduced temperature and/or increased pressure at which the gas molecules lose their kinetic energy to such an extent that they form a regular crystalline lattice or a compact solid structure.
The mechanism of resublimation follows from the principles of thermodynamics and describes phenomena in which a system seeks to minimise internal energy by reducing volume and maximising intermolecular interactions. A characteristic aspect of this process is the release of heat of resublimation, analogous to the heat of condensation or solidification, which must be dissipated from the system to ensure the stability of the newly formed solid phase.
In molecular terms, resublimation involves a sudden reduction in the translational freedom of gas molecules, which, under the influence of reduced thermal energy and increased van der Waals forces or chemical bonds, begin to arrange themselves into ordered crystalline structures. This process plays a key role in many natural phenomena, such as the formation of frost, the formation of ice on surfaces and the deposition of molecules in high mountain atmospheres.
In industrial technologies, resublimation is used in the purification of chemicals, including the fractional distillation of solids and in sublimation thin film deposition (PVD - Physical Vapour Deposition), where the controlled transition of gas to solids enables the production of coatings with precisely defined morphology and chemical composition.
In analytical chemistry, the resublimation process is used in methods for the separation and purification of low-volatility chemicals, where the selective condensation of substance vapours allows their separation from mixtures. In microelectronics and nanotechnology controlled resublimation is used for the deposition of thin-film functional materials on semiconductor substrates and in the design of optoelectronic devices.
Resublimation parameters, such as resublimation pressure and deposition temperature, depend on the characteristics of the substance, its triple point and specific molecular properties, including polarity, molar mass and intermolecular bond strength. Precise control of this process requires advanced temperature control systems, vacuum systems and crystallisation analysis methods that ensure reproducibility and high quality of the solid phases obtained.
Transfer Multisort Elektronik (TME) is one of the world’s largest global distributors of electronic components, electrotechnical parts, workshop equipment, and industrial automation. The catalog includes over 1,500,000 products from 1,300 leading manufacturers. TME’s modern logistics centers in Łódź and Rzgów (Poland), with a combined area of over 40,000 m², ship nearly 6,000 packages daily to customers in more than 150 countries.
TME also invests in the development of knowledge and skills of young engineers and electronics enthusiasts through the TME Education project, and supports the tech community by organizing the TechMasterEvent series, promoting innovation and experience exchange.