+1 500 000 products in offer

7000 packages per day

+300 000 clients from 150 countries

Quick Buy Favourites
Cart

Equivalent diagram (equivalent circuit) - definition

An equivalent circuit diagram is a simplified, analytical representation of a real object - a component, system or technical system - expressed by means of idealised mathematical and physical models and components, such as resistors, voltage sources, Capacitors, inductors, generators or transformers. Its main objective is to represent the basic functional properties of the analysed system in a way that allows easy calculation, simulation and evaluation of the system's behaviour under specific operating conditions.

In electrical engineering and electronics, equivalent diagrams are used to represent real-world components - such as transmission lines, transformers, electrical machines, power sources or semiconductor devices - by means of a set of simple passive and active elements. For example, a transformer can be represented by a model including winding resistance, distributed inductances and parasitic capacitances, which allows the analysis of losses, voltage drops or frequency characteristics.

The equivalent diagram can be linear or non-linear, depending on the scope and accuracy of the model. It also often comes in static forms (for steady-state analysis) or dynamic forms (taking into account time variables). In Automation and control theory these schemes are used to represent the dynamics of processes and control objects in the form of transmittance models or differential equations.

The advantage of using surrogate diagrams is that complex systems can be replaced by their simplified representation, which allows a quick analysis of the system's behaviour using classical analytical, numerical or simulation methods. This makes them an indispensable tool in the design, diagnosis and optimisation of technical systems, both in the conceptual and operational phases.

Transfer Multisort Elektronik (TME) is one of the world’s largest global distributors of electronic components, electrotechnical parts, workshop equipment, and industrial automation. The catalog includes over 1,500,000 products from 1,300 leading manufacturers. TME’s modern logistics centers in Łódź and Rzgów (Poland), with a combined area of over 40,000 m², ship nearly 6,000 packages daily to customers in more than 150 countries.

TME also invests in the development of knowledge and skills of young engineers and electronics enthusiasts through the TME Education project, and supports the tech community by organizing the TechMasterEvent series, promoting innovation and experience exchange.

READ ALSO