+1 500 000 products in offer
7000 packages per day
+320 000 clients from 150 countries
Steady state is a concept in the field of analysis of dynamic, electrical, mechanical and thermal systems, denoting such a state of operation of a system in which all variables describing its behaviour reach constant or periodically recurring values and cease to depend on time in a transient manner. In the context of system response analysis, steady state follows a transient phase in which the system responds to a change in the initial conditions or input signal.
In linear systems, steady state is achieved by a constant or periodic forcing, e.g. a sinusoidal or step voltage. Characteristically, in steady state the response of the system becomes predictable and described only by the input parameters and the properties of the system itself, regardless of the initial conditions. For systems described by differential or differential equations, this means that the general solution converges to a forced solution over time, while the free components - which depend on the initial condition - vanish.
Steady state is crucial in the analysis and design of technical devices, as it allows their performance to be assessed under nominal conditions, as well as simplifying the equations describing the behaviour of the system. In electrical engineering refers, among other things, to the stable values of voltages and currents in circuits after the transients associated with inductance and capacitance have ceased. In Automation and control theory it allows the evaluation of control accuracy and static error. For periodic systems, such as filters or power electronic converters, the steady state can be cyclic, reflecting synchronisation with the input signal.
Transfer Multisort Elektronik (TME) is one of the world’s largest global distributors of electronic components, electrotechnical parts, workshop equipment, and industrial automation. The catalog includes over 1,500,000 products from 1,300 leading manufacturers. TME’s modern logistics centers in Łódź and Rzgów (Poland), with a combined area of over 40,000 m², ship nearly 6,000 packages daily to customers in more than 150 countries.
TME also invests in the development of knowledge and skills of young engineers and electronics enthusiasts through the TME Education project, and supports the tech community by organizing the TechMasterEvent series, promoting innovation and experience exchange.