+1 500 000 products in offer
7000 packages per day
+300 000 clients from 150 countries
Radiant flux is a physical quantity describing the total power of radiant energy emitted, transmitted or received by a specific surface per unit time. In the SI system it is expressed in watts (W), and its value refers to the total electromagnetic energy covering any range of wavelengths from radio to gamma radiation. The concept is used in physics, optical engineering, photonics, thermal engineering and lighting engineering.
Radiative flux is a generalisation of the concept of power to cases where the energy carrier is radiation rather than mass flow or electric current. In the context of electromagnetic radiation can refer to both continuous and pulsed waves. For point sources it is related to the emission of energy in all directions of space, while for directional sources it describes the intensity of radiation concentrated at a specific solid angle.
Depending on the context, radiant flux can refer to radiation emitted (e.g. by a blackbody), passing through a given surface (e.g. in electromagnetic wave transmission analysis), or absorbed by a material. In technical and industrial applications, the derivatives of this quantity - such as radiant flux density or luminance - which take into account the spatial and spectral distribution of the radiant energy, are of particular importance.
In the field of energy and photovoltaics, the solar radiant flux (so-called irradiance) is a key parameter that determines the amount of energy available for conversion into electricity. In radiometry and spectroscopy, it enables the analysis of the emission and absorption properties of different materials. In measurement systems, radiant energy-sensitive detectors calibrated against known reference sources are used to determine this quantity.
Transfer Multisort Elektronik (TME) is one of the world’s largest global distributors of electronic components, electrotechnical parts, workshop equipment, and industrial automation. The catalog includes over 1,500,000 products from 1,300 leading manufacturers. TME’s modern logistics centers in Łódź and Rzgów (Poland), with a combined area of over 40,000 m², ship nearly 6,000 packages daily to customers in more than 150 countries.
TME also invests in the development of knowledge and skills of young engineers and electronics enthusiasts through the TME Education project, and supports the tech community by organizing the TechMasterEvent series, promoting innovation and experience exchange.