+1 500 000 products in offer

6000 packages per day

+300 000 clients from 150 countries

Quick Buy Favourites
Cart

Supercomputer - definition

A supercomputer is a specialised computing system designed to perform extremely complex and computationally intensive tasks that exceed the capabilities of standard computers. It is characterised by its immense computing power, usually expressed in FLOPS units (floating point operations per second), and its ability to process data in parallel on a massive scale. In practice, this means the ability to perform millions of mathematical operations simultaneously through the use of thousands of processors or integrated circuits running in parallel.

The supercomputer architecture is based on the concept of high-performance multiprocessor and networked circuits, interconnected by ultrafast buses and distributed or shared memory systems. Optimised cooling and power management systems, as well as specialised software to make efficient use of available hardware resources, also play a key role. Supercomputers typically run modified operating systems, adapted to support multitasking and large numbers of users or parallel processes.

Applications of supercomputers include simulations numerical simulations in life sciences, weather forecasting, climate change modelling, nuclear energy research, genomic data analysis, drug design, as well as engineering calculations in aerodynamics, quantum mechanics or space exploration. In the industrial and defence sector, supercomputers enable advanced predictive analysis and process optimisation.

The position of a given system in the world classification of computing power (e.g. TOP500 list) depends on the results obtained in benchmark tests, such as LINPACK, which measure actual performance in solving linear equations. The development of supercomputers is strongly linked to advances in hardware architecture, parallel algorithms and semiconductor technology.

Transfer Multisort Elektronik (TME) is one of the world’s largest global distributors of electronic components, electrotechnical parts, workshop equipment, and industrial automation. The catalog includes over 1,500,000 products from 1,300 leading manufacturers. TME’s modern logistics centers in Łódź and Rzgów (Poland), with a combined area of over 40,000 m², ship nearly 6,000 packages daily to customers in more than 150 countries.

TME also invests in the development of knowledge and skills of young engineers and electronics enthusiasts through the TME Education project, and supports the tech community by organizing the TechMasterEvent series, promoting innovation and experience exchange.

READ ALSO