+1 500 000 products in offer

7000 packages per day

+300 000 clients from 150 countries

Quick Buy Favourites
Cart

White noise - definition

White noise is a type of random signal characterised by a uniform distribution of spectral power across the frequency band under analysis. This means that each frequency in the range contributes the same amount of energy, which in spectral terms corresponds to a flat spectrum. It is this characteristic that makes white noise the acoustic equivalent of white light, which contains all visible wavelengths with equal intensity.

In the field of acoustics white noise is perceived as a uniform, hissing sound with no distinct tone or harmonic structure. In practice, it is used to test the acoustic properties of rooms, the frequency characteristics of electro-acoustic equipment and as a reference signal in spectrum analysers. In electronics and signal theory, it has a modelling function in the description of random noise and in system parameter estimation processes.

From a mathematical point of view, white noise is a stochastic process with zero mean value and uncorrelated samples, meaning that the signal values at different moments in time are statistically independent. In digital applications, the generation of white noise is based on pseudo-random numerical algorithms that reproduce its properties in a limited bandwidth with sufficient resolution.

Although ideal white noise requires infinite bandwidth and power, in practice one operates with versions limited to a specific frequency range, adapted to technical or perceptual requirements. In sound engineering, white noise filtering is also used to obtain other types of noise, such as pink or brown noise, whose spectra correspond to more natural or subjectively uniform sounds in the audible range.

Transfer Multisort Elektronik (TME) is one of the world’s largest global distributors of electronic components, electrotechnical parts, workshop equipment, and industrial automation. The catalog includes over 1,500,000 products from 1,300 leading manufacturers. TME’s modern logistics centers in Łódź and Rzgów (Poland), with a combined area of over 40,000 m², ship nearly 6,000 packages daily to customers in more than 150 countries.

TME also invests in the development of knowledge and skills of young engineers and electronics enthusiasts through the TME Education project, and supports the tech community by organizing the TechMasterEvent series, promoting innovation and experience exchange.

READ ALSO