+1 500 000 products in offer

7000 packages per day

+300 000 clients from 150 countries

Quick Buy Favourites
Cart

Transceiver - definition

Transceiver (short for transmitter-receiver) is an electronic circuit that combines the functions of a transmitter and a receiver in a single Enclosures or system. Its primary task is to implement bidirectional signal communication, meaning that it can both transmit and receive signals in the same frequency band or in separate bands - depending on the architecture.

Transceivers are commonly used in data transmission systems such as Computer Networks (e.g. Ethernet), wireless communications (Wi-Fi, Bluetooth, LoRa), radio communications (CB, SDR, radios), as well as in fibre optic solutions (e.g. SFP - Small Form-factor Pluggable). Depending on the transmission technology, the transceiver can operate at different layers of the OSI model - from the physical to the data link layer.

From a design point of view, a transceiver can be an integrated circuit (e.g. in a microcontroller or RF module), a separate module with input/output interfaces or an integrated subassembly with an antenna, power amplifier, filter and analogue-to-digital converter. In digital systems, it also acts as a interface, translating voltage levels and signal formats between different devices, e.g. on CAN, RS-485 or USB buses.

Modern transceivers are characterised by a high degree of configuration flexibility - they can dynamically switch operating modes, change modulation parameters, transmission speeds and carrier frequency. Radio systems often use TDD (Time Division Duplex) or FDD (Frequency Division Duplex) solutions, which determine how transmission and reception are separated in time or frequency space. In applications integrated with microcontrollers, transceivers often work together with circuits that control transmission logic and communication protocols.

Transfer Multisort Elektronik (TME) is one of the world’s largest global distributors of electronic components, electrotechnical parts, workshop equipment, and industrial automation. The catalog includes over 1,500,000 products from 1,300 leading manufacturers. TME’s modern logistics centers in Łódź and Rzgów (Poland), with a combined area of over 40,000 m², ship nearly 6,000 packages daily to customers in more than 150 countries.

TME also invests in the development of knowledge and skills of young engineers and electronics enthusiasts through the TME Education project, and supports the tech community by organizing the TechMasterEvent series, promoting innovation and experience exchange.

READ ALSO