+1 500 000 products in offer

7000 packages per day

+300 000 clients from 150 countries

Quick Buy Favourites
Cart

UMTS (Universal Mobile Telecommunications System) - definition

UMTS (Universal Mobile Telecommunications System) is a third-generation (3G) standard for mobile phone systems, developed under the International Telecommunications Union (ITU) IMT-2000 initiative and developed by the 3rd Generation Partnership Project (3GPP) organisation. Its primary objective was to provide significantly higher bandwidth and quality of data and voice services compared to second generation systems (GSM), while maintaining compatibility with existing infrastructure.

UMTS uses the Wideband Code Division Multiple Access (WCDMA) radio access technique, which enables the simultaneous transmission of multiple signals in the same frequency band, using user separation codes. Such technology ensures better use of available radio resources, greater resistance to interference and more flexible management of network traffic. UMTS usually operates in the 2100 MHz bands, although it is also possible to operate in other bands, depending on the region and spectrum availability.

The UMTS network structure consists of several functional layers, including the radio layer (UTRAN - UMTS Terrestrial Radio Access Network), the core network and service management systems. The introduction of packet technology (e.g. HSPA - High Speed Packet Access) made it possible to achieve transmission speeds of up to several megabits per second, making it possible to support multimedia applications, video conferencing, mobile Internet and location-based services.

UMTS represented an important transition stage between classic voice systems and modern broadband solutions such as LTE and 5G. Thanks to its flexible architecture and modular design, it was progressively developed and integrated into subsequent generations, enabling a smooth transition of operators and users to more advanced mobile communication technologies.

Transfer Multisort Elektronik (TME) is one of the world’s largest global distributors of electronic components, electrotechnical parts, workshop equipment, and industrial automation. The catalog includes over 1,500,000 products from 1,300 leading manufacturers. TME’s modern logistics centers in Łódź and Rzgów (Poland), with a combined area of over 40,000 m², ship nearly 6,000 packages daily to customers in more than 150 countries.

TME also invests in the development of knowledge and skills of young engineers and electronics enthusiasts through the TME Education project, and supports the tech community by organizing the TechMasterEvent series, promoting innovation and experience exchange.

READ ALSO