+1 500 000 products in offer

7000 packages per day

+300 000 clients from 150 countries

Quick Buy Favourites
Cart

Uninterruptible power supply (UPS) - definition

Uninterruptible Power Supplies (UPS), Uninterruptible Power Supply) is an electrical device that ensures continuity of power supply in the event of mains voltage failure or instability. Its operation is based on the conversion of energy stored in internal batteries into output voltage with stabilised characteristics, which protects critical equipment from the effects of sudden power cuts, voltage drops and electromagnetic interference.

The UPS system architecture comprises a rectifier, which converts alternating voltage to direct voltage to charge the batteries, an inverter which is responsible for generating the output voltage during a fault, and control systems that manage switching between operating modes. Depending on the topology of the UPS system, there are offline models, line-interactive and online (VFI) models, differ in their voltage regulation mechanism, speed of changeover to emergency power supply and ability to eliminate harmonic disturbances.

In offline systems, also called standby, rechargeable Batteries are only supplied when a mains power failure is detected, which results in a brief interruption of power supply due to the relay switching time. Line Supplies-interactive power supplies use automatic voltage regulation (AVR), allowing output voltage stabilisation without having to switch to battery mode, which increases their efficiency and reduces cell wear and tear. Online designs operate in double conversion mode, where the AC voltage is continuously converted to DC voltage and again to AC voltage, which completely isolates connected equipment from mains disturbances and provides instantaneous switching to battery power without switching delays.

Power Supplies are used in critical systems, such as IT infrastructure, server rooms, industrial automation systems and medical devices, where even short interruptions in the power supply can lead to serious operational losses. High-performance industrial models are equipped with energy management systems, high-performance industrial models are equipped with energy management systems allowing interaction with power generators and the implementation of load management strategies based on algorithms predictive algorithms and power quality analysis.

Advanced UPS units integrate communication technologies, technologies such as SNMP, Modbus or USB, for remote monitoring of operating parameters and automatic shutdown and restart of protected systems. The use of modern lithium-ion Rechargeable Batteries-ion batteries and supercapacitor technology supercapacitors technology technology allows an increase in the system's lifetime and a reduction in charging time compared to traditional lead-acid cells-lead-acid cells. Active power factor correction (PFC) and energy optimisation mechanisms reduce thermal losses and increase power conversion efficiency, resulting in improved operational efficiency and lower operating costs.

UPS systems may be configured in redundant systems (N+1), where multiple units operate in parallel to maximise reliability and eliminate single points of failure. Modern data centres also use modular UPS architectures, are also being used in modern data centres to enable power scaling and dynamic adjustment of power energy storage according to the changing demands of the system. High resistance to environmental conditions and the ability to work with renewable energy sources make, make uninterruptible power supplies a key component of the infrastructure for ensuring business continuity of high-availability systems.

Transfer Multisort Elektronik (TME) is one of the world’s largest global distributors of electronic components, electrotechnical parts, workshop equipment, and industrial automation. The catalog includes over 1,500,000 products from 1,300 leading manufacturers. TME’s modern logistics centers in Łódź and Rzgów (Poland), with a combined area of over 40,000 m², ship nearly 6,000 packages daily to customers in more than 150 countries.

TME also invests in the development of knowledge and skills of young engineers and electronics enthusiasts through the TME Education project, and supports the tech community by organizing the TechMasterEvent series, promoting innovation and experience exchange.

READ ALSO