+1 500 000 products in offer

7000 packages per day

+300 000 clients from 150 countries

Quick Buy Favourites
Cart

Pressure under control – the role of pressure transducers in industrial systems.

Date of publication: 30-10-2025 🕒 9 min read

In the world of automation and process engineering, pressure transmitters are among those components that – although often invisible – play a crucial role in ensuring the safety and efficiency of installations. From oil refineries to hydroelectric power plants, from HVAC systems to aviation – wherever pressure needs to be precisely monitored and controlled, these devices become indispensable.

In this article, we look at how pressure transmitters work, what types are available on the market, and how they differ from sensors. We will also discuss their applications in various industrial sectors, additional functions found in modern designs, and technological trends shaping the future of pressure measurement. This is a practical guide for engineers, system designers, and industrial users seeking reliable solutions for their applications.

Key Information in brief

  • Pressure transmitters convert pressure values into electrical signals, enabling monitoring and control of industrial processes.
  • There are relative, absolute, and differential pressure transmitters, selected depending on the application type.
  • Modern pressure transmitters offer additional features such as environmental condition compensation and auto-calibration.
  • In petrochemicals, energy, HVAC, and automotive sectors, they play a crucial role in controlling operational parameters of installations.
  • Pressure transmitters differ from sensors and transmitters in functionality and the way signals are processed and transmitted.

Principle of operation of pressure transmitters

Pressure transmitters are key elements in industrial automation systems, responsible for precisely converting pressure values into electrical signals. This process is based on the use of material properties reacting to mechanical stress or displacement caused by pressure.

The basic operating mechanism is that pressure acting on a membrane or other measuring element causes its deformation. The resulting deformation is then converted into an electrical signal, whose value corresponds to the measured pressure. Depending on the design, this can be a voltage signal (mV or V), current (e.g., 4–20mA), or digital.

Pressure Transmitters

A typical pressure transmitter consists of two main parts: the measuring element and the electronic system.

  • The measuring element (sensor) registers the pressure and responds by changing physical properties, such as resistance in strain gauge sensors or capacitance in capacitive solutions.
  • The processing electronics amplify the sensor signal, compensate for external factors, and prepare an output signal compatible with control systems.

In more advanced designs, the electronic system may also implement additional functions such as auto-calibration, error detection (i.e., detecting incorrect readings and warning the user), or digital communication with superior devices in the industrial network.

Types of output signals

Pressure transmitters provide various types of output signals, allowing adaptation to the specifics of control systems and installation conditions. In industrial systems, analog signals dominate, such as voltage signals within millivolt or volt ranges and current signals, most commonly 4–20mA. Current signals are particularly valued in applications with long distances between the transmitter and controller because they are less susceptible to electromagnetic interference and voltage drops along cables.

Digital signals are increasingly playing a greater role, enabling the transmission of additional diagnostic data alongside measurement values. Popular solutions are based on communication protocols such as Modbus or CAN, used in automation and automotive industries. In modern plants utilizing the Industry 4.0 concept, pressure transmitters can be integrated with IoT networks, enabling remote real-time parameter monitoring.

Calibration and influence of external actors

To maintain high measurement accuracy, periodic calibration of the pressure transmitter is necessary. This process involves comparing device readings with reference values and applying corrections if necessary. Regular checking of operational parameters is especially important in environments where the device is exposed to changing ambient conditions.

External factors such as temperature, humidity, or mechanical vibrations can affect the stability and repeatability of the output signal. Therefore, modern transmitters are equipped with systems compensating for temperature changes and filters damping the effect of vibrations. Applications requiring the highest precision use devices with a high accuracy class, compliant with international standards like ISO 9001 or European CEN standards, which specify calibration procedures and permissible measurement deviations.

Types of pressure transmitters

Pressure transmitter

The basic type of devices used in industry are pressure transmitters that enable measurement of various kinds of pressure. These transmitters can measure relative pressure, referring the value to atmospheric pressure, typical for hydraulic and pneumatic systems. Versions for measuring absolute pressure are used where the reference is absolute vacuum, for example in vacuum processes or monitoring technological gases.

Differential pressure transmitter

Differential pressure transmitters are primarily used in systems requiring continuous monitoring of pressure differences. A typical example is filtration systems, where they help detect pressure drops across filters, indicating the need for replacement. In HVAC installations, these transmitters control pressure differences between rooms or sections of ventilation ducts, which is vital for maintaining proper operating conditions of air conditioning systems. In technological processes, they enable precise control of flow and pressure in reactors or pipelines.

Differential Pressure Transmitters

Air velocity transmitter

A specialized type are air velocity transmitters, used to measure flow and dynamic pressure in air ducts. These devices, often based on the Pitot principle, allow accurate control of ventilation and air conditioning systems. They are also employed in industrial systems where monitoring airflow velocity in technological processes or environmental measurements is required.

Air Velocity Transmitters

Comparison of pressure transmitter types

Transmitter Type Measurement Ranges Advantages Limitations
Pressure Transmitter from absolute vacuum to several hundred MPa Versatility, wide application range Requires temperature compensation with large ambient changes
Differential Transmitter mbar to hundreds of bar pressure difference Precise measurement of pressure drops in installations Sensitive to mechanical disturbances and vibrations
Air Velocity Transmitter several m/s to several dozen m/s Ideal for HVAC systems and flow monitoring Limited to air and gases

As shown in the table above, each transmitter type finds its place in specific industrial applications. To better understand where and how they are used, it is worth examining the different types of pressure monitored in these systems.

Controlled quantities and their importance in industrial applications

Relative pressure

Relative pressure is the most commonly measured parameter in industrial systems. It defines the difference between the measured pressure and atmospheric pressure, which serves as a reference point for most technological processes. This measurement method allows continuous monitoring of operating parameters in installations where atmospheric conditions may vary but do not critically impact the process itself.

In hydraulic installations, relative pressure transmitters control working pressure in pipelines, protecting systems from exceeding limit values. In industrial pneumatics, their task is to oversee compressed air pressure, allowing for optimal efficiency of systems powering actuators, valves, and other actuating elements. Due to their simplicity and versatility, sensors of this type are a primary choice in many industrial applications where fast response to working pressure fluctuations is essential.

Transmitters with Relative Pressure Control

Absolute pressure

Absolute pressure is measured relative to absolute vacuum, meaning the reference point is the absence of any pressure. This measurement type is critical in applications where atmospheric pressure variability might interfere with readings and affect technological processes. Absolute pressure transmitters provide stable results independent of external conditions, which is important in many specialized fields.

In vacuum processes, such transmitters enable precise monitoring of low pressure values, necessary to maintain required product quality, for example in semiconductor or pharmaceutical industries. In petrochemicals, they are used to monitor pressure in tanks and pipelines, where accurate absolute measurement is essential for operational safety and optimizing performance of gas and liquid processes under high pressure.

Transmitters with Absolute Pressure Control

Differential pressure

Differential pressure defines the difference in values between two points in a system and is a key parameter in applications requiring precise flow control or system state monitoring. Differential pressure transmitters are often used to monitor filter contamination. When the pressure difference before and after a filter exceeds a set value, it signals the need for maintenance or filter replacement.

In liquid level measurements in tanks, differential pressure allows determining the liquid column height by using the pressure difference at the tank bottom and a reference point. This method is especially useful in closed or pressurized tanks.

In the energy sector, differential transmitters support flow control in steam and cooling systems, where pressure differences indicate performance of heat exchangers or circulation pumps. In the chemical industry, they enable safe process management in reactors, distillation columns, and pipelines, where accurate monitoring of pressure differences is vital to avoid failures or product loss.

Industrial applications of pressure transmitters

Petrochemical and chemical industry

In the petrochemical and chemical sectors, pressure transmitters are indispensable components of process control systems. They allow real-time pressure monitoring in installations transporting gases and liquids, in high-pressure reactors, and distillation columns. This makes it possible to maintain stable process conditions, which are critical for production quality and safety.

Transmitters also function as safety elements, cooperating with safety valves and shutoff systems. In the event of sudden pressure changes, they can trigger emergency procedures, minimizing the risk of hazardous substance leaks and installation damage.

Energy and hydropower

In conventional and renewable energy sectors, pressure transmitters serve for precise measurement of parameters in key system components. Pressure control in steam turbines enables optimization of their operation and protection against overloads that could cause mechanical damage.

In hydropower, these devices are used to monitor pressure in pipelines and water reservoirs. Maintaining proper pressure values is not only important for turbine efficiency but also for the safety of hydraulic constructions such as dams and barriers.

Industrial automation and industry 4.0

Pressure transmitters have become integral to modern industrial automation systems. Thanks to their integration capability with programmable PLC controllers and Industrial Internet of Things networks, they provide real-time data access. Such solutions enable dynamic production process control and quick response to changing installation conditions.

Within the Industry 4.0 concept, transmitters not only provide measurements but also participate in predictive analysis (i.e., predicting when a device might require servicing), allowing for maintenance planning and minimizing downtime. Their ability to operate in distributed systems makes them key elements in smart factories.

HVAC and building systems

In HVAC installations, pressure transmitters manage air and liquid parameters in ventilation, heating, and air conditioning systems. They help maintain appropriate pressure differences in ducts, ensuring efficient operation of heat recovery units, filters, and compressors.

By using these devices, it is also possible to monitor air filter status and regulate water flow in heating and cooling systems. Their presence in building management systems increases user comfort and improves energy efficiency.

Automotive and aviation

In the automotive sector, pressure transmitters are used to monitor engine operating parameters such as fuel, oil, and intake air pressure. Precise measurements allow optimizing combustion and controlling exhaust emissions, which is crucial in modern vehicles.

In aviation, these devices control pressure in fuel, hydraulic, and conditioning systems of aircraft. Their reliability is essential for safety and efficiency during flight, especially under variable atmospheric pressure conditions at high altitudes.

Differences between transmitters and pressure sensors

Can a transmitter function as a sensor?

In many cases, a pressure transmitter acts as a sensor because it contains a measuring element capable of detecting pressure changes. The difference is that a sensor provides a raw signal often needing further processing, while a transmitter converts that signal into a form usable by control or monitoring systems.

Modern transmitters also offer extended features such as temperature compensation, internal diagnostics, and digital communication. This allows them not only to detect pressure changes but also to support more complex operations in integrated automation systems.

Transmitter vs sensor vs transmitter

A pressure sensor is the simplest device that responds to pressure changes and generates a primary signal. A pressure transmitter takes this a step further by converting the signal into a standard electrical output usable in industrial applications. A transmitter also amplifies and sends the signal over longer distances, often using a 4–20mA or digital standard, enabling operation in large installations.

The choice of element depends on the application. Sensors work well in systems where the raw signal can be further processed locally. Transmitters are better suited where a ready signal compatible with control systems is needed. Transmitters find use in extensive industrial networks where resistance to interference and long-distance data transmission are important.

Additional features and advanced solutions

Measurements relative to atmospheric and reference pressure

In many industrial applications, considering variable environmental conditions that can influence measurement accuracy is necessary. Transmitters equipped with atmospheric pressure compensation functions can adjust their readings to current conditions, eliminating errors resulting from external pressure fluctuations. More advanced designs use reference pressure, enabling high stability and repeatability of results regardless of environmental changes.

Intelligent transmitters ("Smart Transducers")

Technological developments have provided pressure transmitters with new capabilities beyond basic measurement. Intelligent versions of these devices offer built-in diagnostics that enable detecting deviations from norms and predicting potential failures. The auto-calibration function maintains high accuracy without manual intervention, significantly simplifying operation and maintenance. Auto-calibration is not standard in all devices—it appears in modern models with HART/Modbus protocol. Wireless communication is also increasingly common, allowing data transmission from transmitters to control systems without needing extensive cabling infrastructure.

Technology development and market trends

Contemporary pressure transmitters follow trends in miniaturization and energy efficiency, allowing their use in compact and mobile measurement systems. Growing importance of renewable energy sources drives demand for solutions suited to these applications' specificities. Transmitters installed in wind turbines or solar systems must have high resistance to variable atmospheric conditions and the ability to operate in remote locations, often powered by limited energy sources.

Summary

Pressure transmitters play a fundamental role in modern industrial systems, enabling precise monitoring and control of processes. A key conclusion is the necessity of conscious device type selection for specific applications. Relative pressure transmitters perform well in hydraulic and pneumatic systems, absolute transmitters are essential in vacuum and petrochemical processes, and differential ones in filter monitoring or liquid level measurement. When choosing a solution, it is worth considering output signal type, additional features, and resistance to environmental factors.

For industrial users and system designers, it is particularly important to take into account normative requirements and installation specifics. Transmitters with compensation and auto-calibration functions can greatly simplify operation and increase system reliability. In applications requiring long-distance data transmission, considering models with digital or wireless communication that easily integrate with PLC systems and IIoT platforms is advisable. Conscious selection and proper configuration of transmitters guarantee not only safety but also increased efficiency and cost savings in installation operation.

It is worth noting that TME's catalog includes pressure transmitters for industrial applications, meeting high-quality and normative requirements, facilitating selection of the appropriate solution for each application.

Transfer Multisort Elektronik (TME) is one of the world’s largest global distributors of electronic components, electrotechnical parts, workshop equipment, and industrial automation. The catalog includes over 1,500,000 products from 1,300 leading manufacturers. TME’s modern logistics centers in Łódź and Rzgów (Poland), with a combined area of over 40,000 m², ship nearly 6,000 packages daily to customers in more than 150 countries.

TME also invests in the development of knowledge and skills of young engineers and electronics enthusiasts through the TME Education project, and supports the tech community by organizing the TechMasterEvent series, promoting innovation and experience exchange.

rightColumnPicture rightColumnPicture

READ ALSO