+1500000 개 이상의 제품 제공

하루에 7000개의 패키지

150개국에서 28만 명 이상의 고객

Quick Buy 즐겨찾기
카트

자동차 전자기 릴레이

(200)

A relay is an electrical connector with contacts controlled by an electromagnet. Depending on the type, they can be normally open, normally closed or open/closed. The main difference between relays used in electronic devices and automotive relays is in the design. An automotive relay provides an increased guarantee of reliability in a difficult environment (pollution, high temperature, range of temperature changes, mechanical vibrations of different amplitude and frequency), and in case of damage it has to be easily replaced. Some contacts of automotive relays must conduct a significant current which is used to power lighting, window heating, ignition system and other circuits.

To meet such wide requirements, automotive relays are either inserted into a socket or are equipped with disconnectable terminals. They are also equipped with reinforced springs that ensure reliable contact of the contacts even in the presence of vibrations. They often feature an open housing to ensure easy ventilation of the contacts, and to remove the ionized gas between them, which prevents the formation of an electric arc.

Automotive relays – how they are controlled?

Automotive relays are controlled in a similar way as standard electromagnetic relays. Usually, the coil is powered by the voltage available in the vehicle (12V or 24V DC). Relay contacts, depending on their design and purpose, can conduct a current of significant value (even above 100A).

Types of automotive relays

In modern vehicles relays are often used, because not only they switch a significant current, they can also switch low-current circuits. Depending on the intended use, they can be screwed, placed in a socket, equipped with screw terminals or leads adapted to popular slide connectors.

What is more, solid state relays are now commonly used in vehicles, the use of which is easier because in most cases we deal with DC voltage, which is easily commutated with MOS transistors. The relay can have a ventilated or hermetic housing. Many relays used in cars, especially those that connect circuits that carry high current, have an open design.

Basic parameters of relays

The basic parameters of the relay include: contact configuration, maximum load current, coil control voltage, type of housing, relay mounting (socket, panel, soldered, screwed, etc.). Dimensions will also be important in some applications.

How to choose a relay for use in the vehicle?

When selecting an automotive relay for use in a vehicle, the general rules for the relays must be followed. The coil supply voltage will depend on the voltage available in the vehicle installation. The forward current of the contacts and the material from which they are made will be of great importance. Open relays should be used to switch the high-current load, but remember that they should be protected against environmental influences.

제품: 200

창고:

TME
전부
페이지 1
NEW
릴레이: 전자기식; U코일: 12VDC; SPDT; 전원,단안정식; U코일최소: 7.2VDC; 접점: AgSnO2; 10ms
제조업체 부품 번호: HFV15/12-Z1ST-D
제조사: HONGFA RELAY
다음의 수량에 대한 순 가격 300 pcs - 2.29 USD다음의 수량에 대한 총 가격 300 pcs - 2.29 USD
0 TME에 재고 있음
개 번호 (다양성: 60)
최소 주문 수량: 300.
다수: 60.
NEW
릴레이: 전자기식
제조업체 부품 번호: HFV15-P/48-SHST
제조사: HONGFA RELAY
다음의 수량에 대한 순 가격 300 pcs - 3.22 USD다음의 수량에 대한 총 가격 300 pcs - 3.22 USD
0 TME에 재고 있음
개 번호 (다양성: 60)
최소 주문 수량: 300.
다수: 60.
NEW
릴레이: 전자기식; U코일: 12VDC; SPST-NO; 35A; DC 하중 @R: 35A/13.5VDC; 자동차; HFV6
제조업체 부품 번호: HFV6-G/12-HT-D
제조사: HONGFA RELAY
다음의 수량에 대한 순 가격 600 pcs - 2.05 USD다음의 수량에 대한 총 가격 600 pcs - 2.05 USD
0 TME에 재고 있음
개 번호 (다양성: 600)
최소 주문 수량: 600.
다수: 600.
NEW
릴레이: 전자기식; U코일: 12VDC; SPDT; 10A; DC 하중 @R: 35A/13.5VDC; 단안정식,자동차
제조업체 부품 번호: HFV9-G/12-ZS-R
제조사: HONGFA RELAY
다음의 수량에 대한 순 가격 600 pcs - 2.79 USD다음의 수량에 대한 총 가격 600 pcs - 2.79 USD
0 TME에 재고 있음
개 번호 (다양성: 600)
최소 주문 수량: 600.
다수: 600.
NEW
릴레이: 전자기식; U코일: 12VDC; SPST-NO; 자동차; U코일최소: 7.2VDC; HFV16; 90Ω; 1.8W
제조업체 부품 번호: HFV16/12-H1TY-R
제조사: HONGFA RELAY
다음의 수량에 대한 순 가격 300 pcs - 3.02 USD다음의 수량에 대한 총 가격 300 pcs - 3.02 USD
0 TME에 재고 있음
개 번호 (다양성: 300)
최소 주문 수량: 300.
다수: 300.
NEW
릴레이: 전자기식; U코일: 12VDC; SPDT; 전원,단안정식; 90Ω; 1.8W; 접점: AgSnO2; 10ms
제조업체 부품 번호: HFV15/12-Z1TJ-R
제조사: HONGFA RELAY
다음의 수량에 대한 순 가격 300 pcs - 2.14 USD다음의 수량에 대한 총 가격 300 pcs - 2.14 USD
0 TME에 재고 있음
개 번호 (다양성: 60)
최소 주문 수량: 300.
다수: 60.
NEW
릴레이: 전자기식
제조업체 부품 번호: HFV15-P/12-ZST
제조사: HONGFA RELAY
다음의 수량에 대한 순 가격 300 pcs - 2.16 USD다음의 수량에 대한 총 가격 300 pcs - 2.16 USD
0 TME에 재고 있음
개 번호 (다양성: 60)
최소 주문 수량: 300.
다수: 60.
NEW
릴레이: 전자기식; U코일: 24VDC; SPST-NO; 60A; U코일최소: 16VDC; 320Ω; 접점: AgSnO2
제조업체 부품 번호: HFV15/24-H1TJ-D
제조사: HONGFA RELAY
다음의 수량에 대한 순 가격 300 pcs - 1.81 USD다음의 수량에 대한 총 가격 300 pcs - 1.81 USD
0 TME에 재고 있음
개 번호 (다양성: 60)
최소 주문 수량: 300.
다수: 60.
NEW
릴레이: 전자기식; U코일: 12VDC; SPDT; 30A; DC 하중 @R: 20A/13.5VDC; 자동차,초소형
제조업체 부품 번호: HFKC-T/012-ZTC
제조사: HONGFA RELAY
다음의 수량에 대한 순 가격 1200 pcs - 1.86 USD다음의 수량에 대한 총 가격 1200 pcs - 1.86 USD
0 TME에 재고 있음
개 번호 (다양성: 1 200)
최소 주문 수량: 1 200.
다수: 1 200.
NEW
릴레이: 전자기식
제조업체 부품 번호: 45175090175
제조사: HONGFA RELAY
다음의 수량에 대한 순 가격 2000 pcs - 1.66 USD다음의 수량에 대한 총 가격 2000 pcs - 1.66 USD
0 TME에 재고 있음
개 번호 (다양성: 2 000)
최소 주문 수량: 2 000.
다수: 2 000.
NEW
릴레이: 전자기식; U코일: 12VDC; SPST-NO; 70A; DC 하중 @R: 70A/13.5VDC; HFV16
제조업체 부품 번호: HFV16/12-H1ST
제조사: HONGFA RELAY
다음의 수량에 대한 순 가격 300 pcs - 3.02 USD다음의 수량에 대한 총 가격 300 pcs - 3.02 USD
0 TME에 재고 있음
개 번호 (다양성: 300)
최소 주문 수량: 300.
다수: 300.
NEW
릴레이: 전자기식; U코일: 12VDC; SPDT; 30A; 단안정식,자동차; U코일최소: 7.2VDC; HFV6; 90Ω
제조업체 부품 번호: HFV6/012ZS-TD
제조사: HONGFA RELAY
다음의 수량에 대한 순 가격 600 pcs - 2.05 USD다음의 수량에 대한 총 가격 600 pcs - 2.05 USD
0 TME에 재고 있음
개 번호 (다양성: 600)
최소 주문 수량: 600.
다수: 600.
NEW
릴레이: 전자기식; U코일: 12VDC; SPDT; 자동차; U코일최소: 8VDC; HFV6; 124Ω; 접점: AgSnO2
제조업체 부품 번호: HFV6-G/12-ZST-D
제조사: HONGFA RELAY
다음의 수량에 대한 순 가격 600 pcs - 2.55 USD다음의 수량에 대한 총 가격 600 pcs - 2.55 USD
0 TME에 재고 있음
개 번호 (다양성: 600)
최소 주문 수량: 600.
다수: 600.
NEW
릴레이: 전자기식
제조업체 부품 번호: HFV15-P/12-HST
제조사: HONGFA RELAY
다음의 수량에 대한 순 가격 300 pcs - 1.81 USD다음의 수량에 대한 총 가격 300 pcs - 1.81 USD
0 TME에 재고 있음
개 번호 (다양성: 60)
최소 주문 수량: 300.
다수: 60.
NEW
릴레이: 전자기식; U코일: 12VDC; SPST-NO; 전원,단안정식; 90Ω; 1.6W; 접점: AgSnO2; 10ms
제조업체 부품 번호: HFV15/12-H1TJ-D
제조사: HONGFA RELAY
다음의 수량에 대한 순 가격 300 pcs - 1.78 USD다음의 수량에 대한 총 가격 300 pcs - 1.78 USD
0 TME에 재고 있음
개 번호 (다양성: 60)
최소 주문 수량: 300.
다수: 60.
NEW
릴레이: 전자기식; U코일: 12VDC; SPST-NO; 전원,단안정식; U코일최소: 7.2VDC; 90Ω; 1.8W
제조업체 부품 번호: HFV15/12-H5T-R
제조사: HONGFA RELAY
다음의 수량에 대한 순 가격 120 pcs - 2.94 USD다음의 수량에 대한 총 가격 120 pcs - 2.94 USD
0 TME에 재고 있음
개 번호 (다양성: 24)
최소 주문 수량: 120.
다수: 24.
NEW
릴레이: 전자기식; U코일: 12VDC; SPDT; 전원,단안정식; U코일최소: 7.2VDC; 90Ω; 1.6W; 리드: 커넥터
제조업체 부품 번호: HFV15/12-Z1STJ-D
제조사: HONGFA RELAY
다음의 수량에 대한 순 가격 300 pcs - 2.29 USD다음의 수량에 대한 총 가격 300 pcs - 2.29 USD
0 TME에 재고 있음
개 번호 (다양성: 60)
최소 주문 수량: 300.
다수: 60.
NEW
릴레이: 전자기식; U코일: 24VDC; SPDT; U코일최소: 16VDC; 320Ω; 접점: AgSnO2; 플러그인 방식
제조업체 부품 번호: HFV15/24-Z1ST-D
제조사: HONGFA RELAY
다음의 수량에 대한 순 가격 300 pcs - 2.33 USD다음의 수량에 대한 총 가격 300 pcs - 2.33 USD
0 TME에 재고 있음
개 번호 (다양성: 60)
최소 주문 수량: 300.
다수: 60.
NEW
릴레이: 전자기식; U코일: 24VDC; SPDT; 전원,단안정식; U코일최소: 16VDC; 320Ω; 2W; 플러그인 방식
제조업체 부품 번호: HFV15/24-Z1TJ-R
제조사: HONGFA RELAY
다음의 수량에 대한 순 가격 300 pcs - 2.17 USD다음의 수량에 대한 총 가격 300 pcs - 2.17 USD
0 TME에 재고 있음
개 번호 (다양성: 60)
최소 주문 수량: 300.
다수: 60.
NEW
릴레이: 전자기식; U코일: 24VDC; SPDT; U코일최소: 16VDC; 320Ω; 접점: AgSnO2; 플러그인 방식
제조업체 부품 번호: HFV15/24-Z4T
제조사: HONGFA RELAY
다음의 수량에 대한 순 가격 240 pcs - 2.34 USD다음의 수량에 대한 총 가격 240 pcs - 2.34 USD
0 TME에 재고 있음
개 번호 (다양성: 40)
최소 주문 수량: 240.
다수: 40.
표준 오퍼에 포함되지 않은 제품에 대한 요청
요청이 성공적으로 전송되었습니다. 곧 제공된 이메일 주소로 제품 구매 제안서를 보내드리겠습니다.
고객 번호
제조업체 부품 번호
제조 업체
총액
이메일주소
메시지 내용