+1500000 개 이상의 제품 제공

하루에 7000개의 패키지

150개국에서 28만 명 이상의 고객

Quick Buy 즐겨찾기
카트

DC 모터

(1)

Direct current motors (DC motors) convert electrical energy into the rotary motion of the shaft. Unlike servo drives, these motors do not keep information about the current position of the shaft. However, this does not change the fact that they are still widely used due to their simple structure and low costs. TME offers a wide range of DC motors that can be successfully used both in large industrial projects and in the backyard labs of electronics enthusiasts.

DC motors – classification depending on the construction.

In addition to the aforementioned servo drives, there are three most common groups of DC motors:

  • Ferrite core brush-type motors – the most common and simplest type of electric drives. They consist of a ferrite core around which the winding is wound; brushes fed with direct current; winding switching commutator; the stator with permanent magnets and the rotor, i.e. a moving element. Their disadvantage is the relatively quick wear of the brushes and their susceptibility to unfavorable environmental conditions.

  • Brush-type coreless motors – unlike the first group, these drives do not have a core. Instead, the rotor is set in motion; it consists of a winding which in this case is outside the permanent magnets located in the motor housing.

  • Brushless motors – in their case, the mechanical commutator is replaced by an electronic one. This type of an electric motor is characterized by its higher reliability – the lack of contact between the brushes and the commutator means that only the bearings suffer from mechanical wear. However, due to the need for more complex control systems, their cost is higher than in the case of brushed motors.

TME's offers DC motors that can be used in both simple applications and more complex systems. The TME’s catalogue includes the simplest drives that will be used to move a wirelessly controlled car, as well as more advanced motors, e.g. with an integrated encoder, designed for larger-scale projects.

제품: 1

창고:

TME
전부
페이지 1
NEW
전동기: DC; 기어 박스 포함; 24VDC; 200rpm; 50: 1; 축 직경: 6mm; 100mA; 양면 축: 없음
제조사: POLOLU
다음의 수량에 대한 순 가격 1 pcs - 42.31 USD다음의 수량에 대한 총 가격 1 pcs - 42.31 USD
다음의 수량에 대한 순 가격 5 pcs - 37.31 USD다음의 수량에 대한 총 가격 5 pcs - 37.31 USD
다음의 수량에 대한 순 가격 10 pcs - 34.81 USD다음의 수량에 대한 총 가격 10 pcs - 34.81 USD
1 TME에 재고 있음
개 번호 (다양성: 1)
표준 오퍼에 포함되지 않은 제품에 대한 요청
요청이 성공적으로 전송되었습니다. 곧 제공된 이메일 주소로 제품 구매 제안서를 보내드리겠습니다.
고객 번호
제조업체 부품 번호
제조 업체
총액
이메일주소
메시지 내용