+1500000 개 이상의 제품 제공

하루에 7000개의 패키지

150개국에서 28만 명 이상의 고객

Quick Buy 즐겨찾기
카트

접촉기

(1 242)

Contactor – what is a contactor and what is it used for?

A contactor is a type of electric switch. Its design and method of operation are similar to those of an electromagnetic relay. Unlike relays, contactors are used for switching main circuits, while relays – for switching auxiliary circuits. Contactors tolerate electrical surges and overvoltage well. They are characterized by high mechanical durability and allow to achieve a high switching frequency at very high operational reliability.

Contactor – differences between contactors and relays

Contactors differ from the relays not only in terms of their intended use, but also in their construction, as in general they are designed to conduct very high currents. In simple terms, it can be said that although their principle of operation is the same (transmitting an electrical signal after contacts are short-circuited) as that of electromagnetic relays, you can easily distinguish a contactor from a relay at first glance, because usually contactors have a large casing and a distinctive shape.

Contactors are capable of switching highly inductive or capacitive loads. They can be used, for example, to start a powerful electric motor. Relays are used to transmit control signals, including those that switch on the contactor. Relay contacts have a rather small current load capacity (typically up to 10 A) and coil voltage within the range of 5 to 24V. Moreover, a relay has a significantly smaller electromagnet than a contactor, and its contacts do not have any additional devices for electric arc extinguishing.

What is important, the contactor’s contact switching time is longer than in the case of a relay. Contactors (except for the quiet ones) work much louder than the relays.

Contactors – control and power supply methods

A contactor is switched on and powered in the same way as an electromagnetic relay. Its electromagnet is powered with a higher voltage than in the case of a relay. The coil rated voltage in certain versions of a contactor can reach up to 500V DC. Typically used values are: 12V DC/AC, 24V DC/AC, 48V DC, 110V AC, 230V AC.

Contactors – basic parameters

The basic parameters of a contactor include: contact configuration, maximum load current, coil control voltage and insulation voltage. In some applications, additional accessories, such as auxiliary contacts enabling to signal the operation of the contactor or to switch on the auxiliary circuit, will also be very important.

Choosing a right contactor for your application

The choice of a contactor depends on its function, the value of the switched current and voltage, type of voltage (AC/DC) and type of load. In order to choose a right contactor, one should know the circuit parameters mentioned before and choose a contactor with a rated current that is not lower than the one stated there. If used intensively in industrial applications, a contactor with the operating capability of the current specifications should be chosen, in which contacts can handle twice (or more) the load. It prolongs the service life of frequently switched contactors.

A contactor will prove useful in switching electric motors, heaters, pumps, sirens, fluorescent lamps, fans and other high-power electrical equipment

Accessories for contactors

Manufacturers offer many accessories for contactors, for example: auxiliary contacts, mechanical lock-out latches to maintain the contactor status, electronic timer modules to switch the contactor off or on after a certain time and overvoltage protectors.

제품: 1 242

창고:

TME
전부
페이지 1
NEW
GJL1311003R8100 | 접촉기: 3극; NO x3; 보조 접점: NO; 220÷240VAC; 12A; 패널에,DIN 레일 장착용; B7; 커넥터
접촉기: 3극; NO x3; 보조 접점: NO; 220÷240VAC; 12A; 패널에,DIN 레일 장착용; B7; 커넥터
제조업체 부품 번호: GJL1311003R8100
제조사: ABB
다음의 수량에 대한 순 가격 1 pcs - 35.48 USD다음의 수량에 대한 총 가격 1 pcs - 35.48 USD
다음의 수량에 대한 순 가격 4 pcs - 33.60 USD다음의 수량에 대한 총 가격 4 pcs - 33.60 USD
다음의 수량에 대한 순 가격 10 pcs - 31.45 USD다음의 수량에 대한 총 가격 10 pcs - 31.45 USD
0 TME에 재고 있음
개 번호 (다양성: 1)
최소 주문 수량: 1.
다수: 1.
NEW
1SBL137501R1200 | 접촉기: 4극; NC x2 + NO x2; 48÷130VAC,48÷130VDC; 9A; 패널에,DIN 레일 장착용
접촉기: 4극; NC x2 + NO x2; 48÷130VAC,48÷130VDC; 9A; 패널에,DIN 레일 장착용
제조업체 부품 번호: 1SBL137501R1200
제조사: ABB
다음의 수량에 대한 순 가격 1 pcs - 64.77 USD다음의 수량에 대한 총 가격 1 pcs - 64.77 USD
다음의 수량에 대한 순 가격 5 pcs - 60.74 USD다음의 수량에 대한 총 가격 5 pcs - 60.74 USD
다음의 수량에 대한 순 가격 10 pcs - 56.44 USD다음의 수량에 대한 총 가격 10 pcs - 56.44 USD
0 TME에 재고 있음
개 번호 (다양성: 1)
최소 주문 수량: 1.
다수: 1.
NEW
RBS425-22-230V AC | 접촉기: 4극 장치; 25A; 230VAC; NC x2 + NO x2; DIN 레일 장착용; RBS; 리드: 나사 단자
접촉기: 4극 장치; 25A; 230VAC; NC x2 + NO x2; DIN 레일 장착용; RBS; 리드: 나사 단자
제조업체 부품 번호: RBS425-22-230V AC
제조사: ETI POLAM
다음의 수량에 대한 순 가격 1 pcs - 50.02 USD다음의 수량에 대한 총 가격 1 pcs - 50.02 USD
다음의 수량에 대한 순 가격 4 pcs - 46.69 USD다음의 수량에 대한 총 가격 4 pcs - 46.69 USD
다음의 수량에 대한 순 가격 12 pcs - 43.35 USD다음의 수량에 대한 총 가격 12 pcs - 43.35 USD
0 TME에 재고 있음
개 번호 (다양성: 1)
최소 주문 수량: 1.
다수: 1.
NEW
CEC07.01-230V-50/60HZ | 접촉기: 3극; NO x3; 보조 접점: NC; 230VAC; 18A; 패널에,DIN 레일 장착용; CEC; 나사 단자
접촉기: 3극; NO x3; 보조 접점: NC; 230VAC; 18A; 패널에,DIN 레일 장착용; CEC; 나사 단자
제조업체 부품 번호: CEC07.01-230V-50/60HZ
제조사: ETI POLAM
다음의 수량에 대한 순 가격 1 pcs - 21.05 USD다음의 수량에 대한 총 가격 1 pcs - 21.05 USD
다음의 수량에 대한 순 가격 5 pcs - 19.65 USD다음의 수량에 대한 총 가격 5 pcs - 19.65 USD
다음의 수량에 대한 순 가격 10 pcs - 18.25 USD다음의 수량에 대한 총 가격 10 pcs - 18.25 USD
0 TME에 재고 있음
개 번호 (다양성: 1)
최소 주문 수량: 1.
다수: 1.
NEW
EZ9C32220 | 접촉기: 2극 장치; 20A; 220÷230VAC; NO x2; DIN 레일 장착용; IP20; Easy9 EZ; 400V
접촉기: 2극 장치; 20A; 220÷230VAC; NO x2; DIN 레일 장착용; IP20; Easy9 EZ; 400V
제조업체 부품 번호: EZ9C32220
다음의 수량에 대한 순 가격 1 pcs - 21.82 USD다음의 수량에 대한 총 가격 1 pcs - 21.82 USD
다음의 수량에 대한 순 가격 6 pcs - 20.41 USD다음의 수량에 대한 총 가격 6 pcs - 20.41 USD
다음의 수량에 대한 순 가격 12 pcs - 19.00 USD다음의 수량에 대한 총 가격 12 pcs - 19.00 USD
10 TME에 재고 있음
개 번호 (다양성: 1)
최소 주문 수량: 1.
다수: 1.
NEW
GJL1213909R8011 | 접촉기: 3극 역전; NO x3; 보조 접점: NC; 24VDC; 9A; 패널에,DIN 레일 장착용; VBC6; 납땜을 위해
접촉기: 3극 역전; NO x3; 보조 접점: NC; 24VDC; 9A; 패널에,DIN 레일 장착용; VBC6; 납땜을 위해
제조업체 부품 번호: GJL1213909R8011
제조사: ABB
다음의 수량에 대한 순 가격 1 pcs - 78.30 USD다음의 수량에 대한 총 가격 1 pcs - 78.30 USD
다음의 수량에 대한 순 가격 5 pcs - 73.41 USD다음의 수량에 대한 총 가격 5 pcs - 73.41 USD
다음의 수량에 대한 순 가격 10 pcs - 68.51 USD다음의 수량에 대한 총 가격 10 pcs - 68.51 USD
0 TME에 재고 있음
개 번호 (다양성: 1)
최소 주문 수량: 1.
다수: 1.
NEW
GC1620M5 | 접촉기: 2극 장치; 16A; 220÷240VAC; NO x2; DIN 레일 장착용; IP20; TeSys GC; 500V
접촉기: 2극 장치; 16A; 220÷240VAC; NO x2; DIN 레일 장착용; IP20; TeSys GC; 500V
제조업체 부품 번호: GC1620M5
다음의 수량에 대한 순 가격 1 pcs - 40.47 USD다음의 수량에 대한 총 가격 1 pcs - 40.47 USD
다음의 수량에 대한 순 가격 5 pcs - 37.94 USD다음의 수량에 대한 총 가격 5 pcs - 37.94 USD
다음의 수량에 대한 순 가격 10 pcs - 35.41 USD다음의 수량에 대한 총 가격 10 pcs - 35.41 USD
0 TME에 재고 있음
개 번호 (다양성: 1)
최소 주문 수량: 1.
다수: 1.
NEW
3RT2025-1AP00-1AA0 | 접촉기: 3극; NO x3; 보조 접점: NO + NC; 230VAC; 17A; 패널에,DIN 레일 장착용; 3RT20
접촉기: 3극; NO x3; 보조 접점: NO + NC; 230VAC; 17A; 패널에,DIN 레일 장착용; 3RT20
제조업체 부품 번호: 3RT2025-1AP00-1AA0
제조사: SIEMENS
다음의 수량에 대한 순 가격 1 pcs - 53.69 USD다음의 수량에 대한 총 가격 1 pcs - 53.69 USD
다음의 수량에 대한 순 가격 5 pcs - 50.43 USD다음의 수량에 대한 총 가격 5 pcs - 50.43 USD
다음의 수량에 대한 순 가격 10 pcs - 47.17 USD다음의 수량에 대한 총 가격 10 pcs - 47.17 USD
3 TME에 재고 있음
개 번호 (다양성: 1)
최소 주문 수량: 1.
다수: 1.
NEW
3RH2911-2GA31 | 보조 접점; 크기: S00; 스프링 클램프; 정면; 접점: NC + NO x3
보조 접점; 크기: S00; 스프링 클램프; 정면; 접점: NC + NO x3
제조사: SIEMENS
다음의 수량에 대한 순 가격 1 pcs - 11.88 USD다음의 수량에 대한 총 가격 1 pcs - 11.88 USD
다음의 수량에 대한 순 가격 5 pcs - 11.22 USD다음의 수량에 대한 총 가격 5 pcs - 11.22 USD
다음의 수량에 대한 순 가격 10 pcs - 10.49 USD다음의 수량에 대한 총 가격 10 pcs - 10.49 USD
0 TME에 재고 있음
개 번호 (다양성: 1)
최소 주문 수량: 1.
다수: 1.
NEW
CEC09.PR-230V-50/60HZ | 접촉기: 4극; NC x2 + NO x2; 230VAC; 20A; 패널에,DIN 레일 장착용; CEC; 나사 단자
접촉기: 4극; NC x2 + NO x2; 230VAC; 20A; 패널에,DIN 레일 장착용; CEC; 나사 단자
제조업체 부품 번호: CEC09.PR-230V-50/60HZ
제조사: ETI POLAM
다음의 수량에 대한 순 가격 1 pcs - 25.70 USD다음의 수량에 대한 총 가격 1 pcs - 25.70 USD
다음의 수량에 대한 순 가격 5 pcs - 23.99 USD다음의 수량에 대한 총 가격 5 pcs - 23.99 USD
다음의 수량에 대한 순 가격 10 pcs - 22.27 USD다음의 수량에 대한 총 가격 10 pcs - 22.27 USD
0 TME에 재고 있음
개 번호 (다양성: 1)
최소 주문 수량: 1.
다수: 1.
NEW
CEC09.10-48V-DC | 접촉기: 3극; NO x3; 보조 접점: NO; 48VDC; 20A; 패널에,DIN 레일 장착용; CEC; 나사 단자
접촉기: 3극; NO x3; 보조 접점: NO; 48VDC; 20A; 패널에,DIN 레일 장착용; CEC; 나사 단자
제조업체 부품 번호: CEC09.10-48V-DC
제조사: ETI POLAM
다음의 수량에 대한 순 가격 1 pcs - 31.97 USD다음의 수량에 대한 총 가격 1 pcs - 31.97 USD
다음의 수량에 대한 순 가격 5 pcs - 29.83 USD다음의 수량에 대한 총 가격 5 pcs - 29.83 USD
다음의 수량에 대한 순 가격 10 pcs - 27.70 USD다음의 수량에 대한 총 가격 10 pcs - 27.70 USD
0 TME에 재고 있음
개 번호 (다양성: 1)
최소 주문 수량: 1.
다수: 1.
NEW
R 20-02-R-24V AC | 접촉기: 2극 장치; 20A; 24VAC; NC x2; DIN 레일 장착용; R; 리드: 나사 단자; 모듈 수: 1
접촉기: 2극 장치; 20A; 24VAC; NC x2; DIN 레일 장착용; R; 리드: 나사 단자; 모듈 수: 1
제조업체 부품 번호: R 20-02-R-24V AC
제조사: ETI POLAM
다음의 수량에 대한 순 가격 1 pcs - 35.94 USD다음의 수량에 대한 총 가격 1 pcs - 35.94 USD
다음의 수량에 대한 순 가격 5 pcs - 33.54 USD다음의 수량에 대한 총 가격 5 pcs - 33.54 USD
다음의 수량에 대한 순 가격 10 pcs - 31.15 USD다음의 수량에 대한 총 가격 10 pcs - 31.15 USD
0 TME에 재고 있음
개 번호 (다양성: 1)
최소 주문 수량: 1.
다수: 1.
NEW
RD 25-04-R-24V AC/DC | 접촉기: 4극 장치; 25A; 24VAC,24VDC; NC x4; DIN 레일 장착용; RD; 리드: 나사 단자
접촉기: 4극 장치; 25A; 24VAC,24VDC; NC x4; DIN 레일 장착용; RD; 리드: 나사 단자
제조업체 부품 번호: RD 25-04-R-24V AC/DC
제조사: ETI POLAM
다음의 수량에 대한 순 가격 1 pcs - 57.79 USD다음의 수량에 대한 총 가격 1 pcs - 57.79 USD
다음의 수량에 대한 순 가격 5 pcs - 53.94 USD다음의 수량에 대한 총 가격 5 pcs - 53.94 USD
다음의 수량에 대한 순 가격 10 pcs - 50.09 USD다음의 수량에 대한 총 가격 10 pcs - 50.09 USD
0 TME에 재고 있음
개 번호 (다양성: 1)
최소 주문 수량: 1.
다수: 1.
NEW
CECA0.40-24V-50/60HZ | 접촉기: 보조; 보조 접점: NO x4; 24VAC; 10A; 패널에,DIN 레일 장착용; CEC; 나사 단자; W: 48mm
접촉기: 보조; 보조 접점: NO x4; 24VAC; 10A; 패널에,DIN 레일 장착용; CEC; 나사 단자; W: 48mm
제조업체 부품 번호: CECA0.40-24V-50/60HZ
제조사: ETI POLAM
다음의 수량에 대한 순 가격 1 pcs - 21.22 USD다음의 수량에 대한 총 가격 1 pcs - 21.22 USD
다음의 수량에 대한 순 가격 5 pcs - 19.80 USD다음의 수량에 대한 총 가격 5 pcs - 19.80 USD
다음의 수량에 대한 순 가격 10 pcs - 18.39 USD다음의 수량에 대한 총 가격 10 pcs - 18.39 USD
0 TME에 재고 있음
개 번호 (다양성: 1)
최소 주문 수량: 1.
다수: 1.
NEW
RD 25-04-R-230V AC/DC | 접촉기: 4극 장치; 25A; 230VAC,230VDC; NC x4; DIN 레일 장착용; RD; 리드: 나사 단자
접촉기: 4극 장치; 25A; 230VAC,230VDC; NC x4; DIN 레일 장착용; RD; 리드: 나사 단자
제조업체 부품 번호: RD 25-04-R-230V AC/DC
제조사: ETI POLAM
다음의 수량에 대한 순 가격 1 pcs - 47.74 USD다음의 수량에 대한 총 가격 1 pcs - 47.74 USD
다음의 수량에 대한 순 가격 5 pcs - 44.56 USD다음의 수량에 대한 총 가격 5 pcs - 44.56 USD
다음의 수량에 대한 순 가격 10 pcs - 41.38 USD다음의 수량에 대한 총 가격 10 pcs - 41.38 USD
0 TME에 재고 있음
개 번호 (다양성: 1)
최소 주문 수량: 1.
다수: 1.
NEW
CEC07.10-110V-50/60HZ | 접촉기: 3극; NO x3; 보조 접점: NO; 110VAC; 18A; 패널에,DIN 레일 장착용; CEC; 나사 단자
접촉기: 3극; NO x3; 보조 접점: NO; 110VAC; 18A; 패널에,DIN 레일 장착용; CEC; 나사 단자
제조업체 부품 번호: CEC07.10-110V-50/60HZ
제조사: ETI POLAM
다음의 수량에 대한 순 가격 1 pcs - 21.05 USD다음의 수량에 대한 총 가격 1 pcs - 21.05 USD
다음의 수량에 대한 순 가격 5 pcs - 19.65 USD다음의 수량에 대한 총 가격 5 pcs - 19.65 USD
다음의 수량에 대한 순 가격 10 pcs - 18.25 USD다음의 수량에 대한 총 가격 10 pcs - 18.25 USD
0 TME에 재고 있음
개 번호 (다양성: 1)
최소 주문 수량: 1.
다수: 1.
NEW
CEC09.4P-230V-50/60HZ | 접촉기: 4극; NO x4; 230VAC; 20A; 패널에,DIN 레일 장착용; CEC; 나사 단자; W: 48mm; 690V
접촉기: 4극; NO x4; 230VAC; 20A; 패널에,DIN 레일 장착용; CEC; 나사 단자; W: 48mm; 690V
제조업체 부품 번호: CEC09.4P-230V-50/60HZ
제조사: ETI POLAM
다음의 수량에 대한 순 가격 1 pcs - 25.70 USD다음의 수량에 대한 총 가격 1 pcs - 25.70 USD
다음의 수량에 대한 순 가격 5 pcs - 23.99 USD다음의 수량에 대한 총 가격 5 pcs - 23.99 USD
다음의 수량에 대한 순 가격 10 pcs - 22.27 USD다음의 수량에 대한 총 가격 10 pcs - 22.27 USD
0 TME에 재고 있음
개 번호 (다양성: 1)
최소 주문 수량: 1.
다수: 1.
NEW
CEC012.10-48V-50/60HZ | 접촉기: 3극; NO x3; 보조 접점: NO; 48VAC; 22A; 패널에,DIN 레일 장착용; CEC; 나사 단자
접촉기: 3극; NO x3; 보조 접점: NO; 48VAC; 22A; 패널에,DIN 레일 장착용; CEC; 나사 단자
제조업체 부품 번호: CEC012.10-48V-50/60HZ
제조사: ETI POLAM
다음의 수량에 대한 순 가격 1 pcs - 25.30 USD다음의 수량에 대한 총 가격 1 pcs - 25.30 USD
다음의 수량에 대한 순 가격 5 pcs - 23.61 USD다음의 수량에 대한 총 가격 5 pcs - 23.61 USD
다음의 수량에 대한 순 가격 10 pcs - 21.92 USD다음의 수량에 대한 총 가격 10 pcs - 21.92 USD
0 TME에 재고 있음
개 번호 (다양성: 1)
최소 주문 수량: 1.
다수: 1.
NEW
RD 25-40-230V AC/DC | 접촉기: 4극 장치; 25A; 230VAC,230VDC; NO x4; DIN 레일 장착용; RD; 리드: 나사 단자
접촉기: 4극 장치; 25A; 230VAC,230VDC; NO x4; DIN 레일 장착용; RD; 리드: 나사 단자
제조업체 부품 번호: RD 25-40-230V AC/DC
제조사: ETI POLAM
다음의 수량에 대한 순 가격 1 pcs - 39.08 USD다음의 수량에 대한 총 가격 1 pcs - 39.08 USD
다음의 수량에 대한 순 가격 5 pcs - 36.48 USD다음의 수량에 대한 총 가격 5 pcs - 36.48 USD
다음의 수량에 대한 순 가격 10 pcs - 33.87 USD다음의 수량에 대한 총 가격 10 pcs - 33.87 USD
0 TME에 재고 있음
개 번호 (다양성: 1)
최소 주문 수량: 1.
다수: 1.
NEW
CEC09.10-24V-DC | 접촉기: 3극; NO x3; 보조 접점: NO; 24VDC; 20A; 패널에,DIN 레일 장착용; CEC; 나사 단자
접촉기: 3극; NO x3; 보조 접점: NO; 24VDC; 20A; 패널에,DIN 레일 장착용; CEC; 나사 단자
제조업체 부품 번호: CEC09.10-24V-DC
제조사: ETI POLAM
다음의 수량에 대한 순 가격 1 pcs - 31.97 USD다음의 수량에 대한 총 가격 1 pcs - 31.97 USD
다음의 수량에 대한 순 가격 5 pcs - 29.83 USD다음의 수량에 대한 총 가격 5 pcs - 29.83 USD
다음의 수량에 대한 순 가격 10 pcs - 27.70 USD다음의 수량에 대한 총 가격 10 pcs - 27.70 USD
0 TME에 재고 있음
개 번호 (다양성: 1)
최소 주문 수량: 1.
다수: 1.
표준 오퍼에 포함되지 않은 제품에 대한 요청
요청이 성공적으로 전송되었습니다. 곧 제공된 이메일 주소로 제품 구매 제안서를 보내드리겠습니다.
고객 번호
제조업체 부품 번호
제조 업체
총액
이메일주소
메시지 내용