+1500000 개 이상의 제품 제공
하루에 7000개의 패키지
150개국에서 32만 명 이상의 고객
Joysticks are indispensable elements of many machines and devices. Professional manipulators ensure precise simulation of movements and transferring them to the offset of the formed objects. Joysticks are used in such areas as video analysis (tracking systems and camera operation), measuring machines, autonomous robots or medical diagnostics. The main property of joysticks is their precision, which often influences the number of supported axes and stable positions. Depending on the needs, there are also additional buttons that can be used to invoke given functions. During the selection, it is also worth paying attention to the information provided by the manufacturer which concerns mechanical and electrical durability as well as the material from which the body of the element is made. Another important feature is load-bearing capacity in interfaces, which should be adapted to the electronic system. Moreover, work ergonomics may also be important - for example, if a machine operator works in thick gloves, the shape of joystick should be chosen so as not to hinder any movements.
Distributor of electronic components Transfer Multisort Elektronik offers joysticks for various purposes. The product catalogue contains items along with a description and an overview photo. The search engine allows you to narrow browsing to the necessary parameters such as the number of supported axes, stable positions (1-position or 4-position) and mechanical / electrical durability (in terms of working cycles). The description also contains parameters including contact load (into a resistive load) and type of the output. TME distributes products of such manufacturers as Apem, CH Products or Omter TYXN.
창고: