+1 500 000 products in offer

7000 packages per day

+300 000 clients from 150 countries

Quick Buy Favourites
Cart

Fail-safe - definition

Fail-safe, referred to as fail-safe, refers to the concept of designing engineered systems in which a potential failure or loss of functionality results in the transition of a device, component or entire system to a state that minimises risk to people, the environment or infrastructure. Fail-safe mechanisms are an integral part of safety engineering and are used in areas such as industrial automation, rail and air transport, electrical engineering, nuclear power, robotics, information systems and medicine.

The assumption of fail-safe operation is that in the event of an error, power interruption, control signal disconnection or exceeding of limit parameters, the system automatically activates protective mechanisms, e.g. closes a valve, shuts down the power supply, initiates emergency procedures or sets the actuator to the default position. The implementation of fail-safe requires an in-depth hazard analysis (e.g. FMEA, HAZOP) and consideration of redundancy, passive material safety and fault tolerance.

In digital systems fail-safe can be realised through fault detection and self-repair algorithms, hardware watchdogs or data line shorting circuits. In contrast to fail-operational strategies, fail-safe does not guarantee maintenance of functionality, but ensures that safety is maintained as a priority.

Transfer Multisort Elektronik (TME) is one of the world’s largest global distributors of electronic components, electrotechnical parts, workshop equipment, and industrial automation. The catalog includes over 1,500,000 products from 1,300 leading manufacturers. TME’s modern logistics centers in Łódź and Rzgów (Poland), with a combined area of over 40,000 m², ship nearly 6,000 packages daily to customers in more than 150 countries.

TME also invests in the development of knowledge and skills of young engineers and electronics enthusiasts through the TME Education project, and supports the tech community by organizing the TechMasterEvent series, promoting innovation and experience exchange.

READ ALSO