+1 500 000 products in offer

6000 packages per day

+300 000 clients from 150 countries

Quick Buy Favourites
Cart

Commutator - definition

A Commutator is a mechanical-electrical component used mainly in Electric Motors and DC generators, whose function is to periodically change the direction of current flow in the windings of the rotor, so that the electromagnetic torque produced maintains a constant direction. It acts as a rotary contact switch, ensuring a proper connection between the rotating part of the machine and the power supply or energy collection system. The key function of the commutator is to enable the conversion of electrical energy into mechanical energy (in motors) or vice versa (in generators), while maintaining the unidirectional nature of the current in the external circuit.

Structurally, a commutator consists of a set of metal segments, usually made of copper, arranged in a cylindrical form on the rotor axis. These segments are insulated against each other and interact with brushes - contact elements made of a conductive material, usually graphite, which are in constant contact with the rotating segments. As the rotor rotates, the individual commutator segments connect to the Others windings, switching the direction of current in a manner synchronised with the mechanical position.

Commutation, the process of changing the direction of current in the windings, is crucial for maintaining the continuous rotation of the rotor in one direction and for the proper operation of electrical machines. In technical practice, the quality of commutation has a significant impact on the efficiency, durability and level of electromagnetic interference produced by the machine. Commutator malfunctions can lead to sparking, excessive brush wear, and deterioration of the dynamic performance of the drive system.

Although modern designs are increasingly using brushless DC motors with electronic commutation control, the classic commutator is still widely used in simple drives, Electric Motors, household appliances and systems where low cost and simplicity are important. In systems with higher requirements, the use of commutators is limited due to their susceptibility to mechanical wear, maintenance requirements and noise emissions.

Transfer Multisort Elektronik (TME) is one of the world’s largest global distributors of electronic components, electrotechnical parts, workshop equipment, and industrial automation. The catalog includes over 1,500,000 products from 1,300 leading manufacturers. TME’s modern logistics centers in Łódź and Rzgów (Poland), with a combined area of over 40,000 m², ship nearly 6,000 packages daily to customers in more than 150 countries.

TME also invests in the development of knowledge and skills of young engineers and electronics enthusiasts through the TME Education project, and supports the tech community by organizing the TechMasterEvent series, promoting innovation and experience exchange.

READ ALSO