+1 500 000 products in offer
7000 packages per day
+300 000 clients from 150 countries
Static Random Access Memory (SRAM) is a type of ephemeral free-access semiconductor memory that stores data invariably as long as power is supplied. Unlike dynamic memory (DRAM), SRAM does not require periodic refreshing of the contents of the memory cells because the information is stored in the form of stable logic states of bistable circuits, usually made up of six Transistors.
As a result of its design, SRAM is characterised by very fast access times and high operating speeds, making it particularly suitable for applications requiring lightning-fast reading and writing of data. For this reason, it is used, among other things, as cache in microprocessors, data buffers and internal registers. Its structure also provides greater fault tolerance and lower controller complexity compared to dynamic memory.
Technically, each SRAM cell functions as a bistable flip-flop that can maintain one of two logic states without the need for regeneration as long as the supply voltage is maintained. The lack of need for data refresh contributes to the simplicity of the control circuitry, but at the same time increases the area of a single cell, which limits the packing density and capacity of the memory relative to DRAM.
SRAM is an ephemeral memory, meaning that it loses all stored information when power is removed. However, the technology has the advantage of low power consumption in the idle state and immediate access to data, making it ideal for systems where speed and reliability are important. Due to its higher manufacturing cost and larger unit size, SRAM is not used as main memory, but as a specialised component to support processor and high-speed digital circuits.
Transfer Multisort Elektronik (TME) is one of the world’s largest global distributors of electronic components, electrotechnical parts, workshop equipment, and industrial automation. The catalog includes over 1,500,000 products from 1,300 leading manufacturers. TME’s modern logistics centers in Łódź and Rzgów (Poland), with a combined area of over 40,000 m², ship nearly 6,000 packages daily to customers in more than 150 countries.
TME also invests in the development of knowledge and skills of young engineers and electronics enthusiasts through the TME Education project, and supports the tech community by organizing the TechMasterEvent series, promoting innovation and experience exchange.