+1 500 000 products in offer

7000 packages per day

+300 000 clients from 150 countries

Quick Buy Favourites
Cart

Unicode - definition

Unicode is a universal character encoding standard developed to provide a uniform way to represent, process and exchange text across different natural languages and writing systems at a global level. It was designed as an extension of previous spatially limited encoding schemes such as ASCII, and is capable of unambiguously representing the millions of characters, symbols and glyphs used in modern and historical language systems, including the Latin, Cyrillic, Greek, Arabic, Chinese, Devanagari or Korean Hangul alphabets.

The Unicode standard uses code planes, in which characters are assigned to unique code points stored as hexadecimal numbers. The most common encoding implementations are UTF-8, UTF-16 and UTF-32, which differ in the way data is represented in memory and transmission, as well as the degree of spatial efficiency. Unicode defines not only the character set, but also rules for normalisation, sorting, character property classification, type direction and text rendering.

The use of Unicode enables global interoperability of software and information systems, regardless of geographic location, which is essential for international digital communication, natural language processing, databases and web and mobile applications.

Transfer Multisort Elektronik (TME) is one of the world’s largest global distributors of electronic components, electrotechnical parts, workshop equipment, and industrial automation. The catalog includes over 1,500,000 products from 1,300 leading manufacturers. TME’s modern logistics centers in Łódź and Rzgów (Poland), with a combined area of over 40,000 m², ship nearly 6,000 packages daily to customers in more than 150 countries.

TME also invests in the development of knowledge and skills of young engineers and electronics enthusiasts through the TME Education project, and supports the tech community by organizing the TechMasterEvent series, promoting innovation and experience exchange.

READ ALSO