+1 500 000 products in offer
6000 packages per day
+300 000 clients from 150 countries
An actuator is an executive element of an automation system that converts a control signal—typically electrical, pneumatic, or hydraulic—into mechanical motion. Its function is to physically execute a command, such as moving a component, opening a valve, or activating a mechanism, based on instructions received from a controller or a supervisory system.
Actuators are essential components in control and automation systems, enabling these systems to respond to changing conditions in real time. Depending on their design and application, actuators may perform either linear or rotary movements. Common types include electric linear actuators, stepper motors, pneumatic cylinders, and motorized valves. In modern installations, actuators are often integrated with sensors, allowing for precise control and real-time monitoring.
In industrial engineering and robotics, actuators serve as the "muscles" of a device—translating control system decisions into tangible actions. In applications such as building automation, medical equipment, precision optics, or aerospace systems, the choice of a suitable actuator directly impacts the overall system's reliability, accuracy, and responsiveness.
Transfer Multisort Elektronik (TME) is one of the world’s largest global distributors of electronic components, electrotechnical parts, workshop equipment, and industrial automation. The catalog includes over 1,500,000 products from 1,300 leading manufacturers. TME’s modern logistics centers in Łódź and Rzgów (Poland), with a combined area of over 40,000 m², ship nearly 6,000 packages daily to customers in more than 150 countries.
TME also invests in the development of knowledge and skills of young engineers and electronics enthusiasts through the TME Education project, and supports the tech community by organizing the TechMasterEvent series, promoting innovation and experience exchange.