+1 500 000 products in offer

6000 packages per day

+300 000 clients from 150 countries

Quick Buy Favourites
Cart

RAM - definition

RAM (Random-Access Memory) is a type of digital memory that allows direct, random access to any data cell in equal time, regardless of its physical location within the memory structure. RAM is a fundamental component of computer and microprocessor system architecture, serving as the operating memory where data and instructions currently used by the processor are temporarily stored during program execution.

A key characteristic of RAM is its volatility—data stored in memory is lost when power is removed, distinguishing it from non-volatile memories such as ROM, hard drives, or flash memory. Due to its high access speed and ability to be read and written multiple times, RAM plays a critical role in ensuring smooth data processing, system performance, and application responsiveness. Its capacity and speed directly affect a computer’s ability to handle multiple operations simultaneously.

There are two main types of RAM: DRAM (Dynamic RAM), which stores data in capacitors requiring periodic refresh cycles, and SRAM (Static RAM), which uses flip-flops and does not require refreshing but is faster and more expensive to produce. DRAM is commonly used as main memory in personal computers, while SRAM is mainly used in processor cache memory, where high speed is essential.

Modern RAM modules, such as DDR (Double Data Rate), are installed in motherboard slots and operate at defined clock frequencies that determine data bandwidth. These standards continue to evolve toward greater capacity, energy efficiency, and throughput to meet the increasing demands of modern operating systems, multimedia applications, and computing environments. RAM works closely with other computer components to create a dynamic environment for real-time data processing.

Transfer Multisort Elektronik (TME) is one of the world’s largest global distributors of electronic components, electrotechnical parts, workshop equipment, and industrial automation. The catalog includes over 1,500,000 products from 1,300 leading manufacturers. TME’s modern logistics centers in Łódź and Rzgów (Poland), with a combined area of over 40,000 m², ship nearly 6,000 packages daily to customers in more than 150 countries.

TME also invests in the development of knowledge and skills of young engineers and electronics enthusiasts through the TME Education project, and supports the tech community by organizing the TechMasterEvent series, promoting innovation and experience exchange.

READ ALSO