+1 500 000 products in offer
7000 packages per day
+300 000 clients from 150 countries
Router is a network device used to connect different segments of computer networks and direct data traffic between them based on logical addresses, typically using the IP protocol. Its primary function is to analyze network packets and determine their forwarding path, enabling efficient communication between devices in different subnets, as well as between local networks and the Internet.
A router acts as an intermediary node in data transmission, equipped with software that allows for dynamic or static routing of network packets. This process, known as routing, relies on routing tables containing information about available paths, their costs, and preferences. Using these tables, the router can deliver data to the destination while selecting the optimal transmission route, even within complex network topologies.
In home and office environments, routers often provide additional functions by integrating a switch, Wi-Fi access point, firewall, DHCP server, and Network Address Translation (NAT) within a single unit. This simplifies network traffic management and allows multiple devices to access the Internet simultaneously. In more advanced systems, routers support dynamic routing protocols, load balancing, and security policy configuration.
Routers operate at the third layer of the OSI model (network layer), distinguishing them from switches and bridges that function at lower layers. In industrial, corporate, and service provider applications, high-performance routers are used for their robustness, interference resistance, and ability to handle multiple interfaces simultaneously. Their importance continues to grow with the expansion of wide area networks, virtualization, IoT, and cloud services, where reliable communication between distributed resources is crucial for the continuity of IT systems.
Transfer Multisort Elektronik (TME) is one of the world’s largest global distributors of electronic components, electrotechnical parts, workshop equipment, and industrial automation. The catalog includes over 1,500,000 products from 1,300 leading manufacturers. TME’s modern logistics centers in Łódź and Rzgów (Poland), with a combined area of over 40,000 m², ship nearly 6,000 packages daily to customers in more than 150 countries.
TME also invests in the development of knowledge and skills of young engineers and electronics enthusiasts through the TME Education project, and supports the tech community by organizing the TechMasterEvent series, promoting innovation and experience exchange.