+1 500 000 products in offer
7000 packages per day
+300 000 clients from 150 countries
The Nyquist Frequency is a concept in the theory of signal processing, which defines the maximum frequency of the component of an analogue signal that can be correctly reproduced with digital sampling. It is equal to half the sampling frequency, which is the number of samples taken from the signal per unit time. According to the Nyquist-Shannon theorem, in order to avoid distortion when reconstructing a signal from samples, it is necessary to sample it at a frequency at least twice as high as the highest frequency present in that signal.
This concept plays a fundamental role in analogue-to-digital conversion (ADC) systems, data transmission and digital audio and video processing. In practice, the use of a sampling frequency higher than that required by the Nyquist frequency provides a margin of safety and reduces the risk of aliasing - a phenomenon involving the overlapping of signal spectra, which leads to the loss of information and the generation of spurious components in the reconstructed signal.
The Nyquist frequency is not the same as the maximum frequency of the signal analysed, but is a limit value that this signal should not exceed in order to comply with the accepted sampling frequency. In digital systems, additional anti-aliasing filters are used to attenuate signal components above this limit even before sampling.
This concept also has applications in discrete systems theory, spectral analysis and the design of digital filters. Knowledge of the Nyquist frequency is crucial in the design of measurement systems, data acquisition and information processing, where maintaining the integrity of the original signal is important for the quality of the final result.
Transfer Multisort Elektronik (TME) is one of the world’s largest global distributors of electronic components, electrotechnical parts, workshop equipment, and industrial automation. The catalog includes over 1,500,000 products from 1,300 leading manufacturers. TME’s modern logistics centers in Łódź and Rzgów (Poland), with a combined area of over 40,000 m², ship nearly 6,000 packages daily to customers in more than 150 countries.
TME also invests in the development of knowledge and skills of young engineers and electronics enthusiasts through the TME Education project, and supports the tech community by organizing the TechMasterEvent series, promoting innovation and experience exchange.