+1 500 000 products in offer

7000 packages per day

+300 000 clients from 150 countries

Quick Buy Favourites
Cart

Standing wave - definition

A Standing Wave is a special case of the interference of two waves of the same frequency, amplitude and direction of polarisation, travelling in opposite directions in the same medium. Their overlap results in a non-diverging system of oscillations in which alternating areas of maximum amplification (arrows) and total extinction (nodes) are observed. A characteristic feature of a standing wave is that energy is not transferred through the medium in the direction of propagation, but oscillates locally around equilibrium points.

Mathematically, a standing wave is described as the sum of two oppositely running harmonic waves. Its spatial profile remains constant over time, while the amplitude of oscillation at individual points varies periodically according to a function of time. The nodes of the wave are the locations where the amplitude of oscillation is zero at any time, while the arrows are the points of maximum excursion where mechanical or electromagnetic energy locally concentrates.

The standing wave phenomenon appears in Others in physics, including acoustics, optics, electronics and wave mechanics. In waveguides, transmission lines, musical instruments or resonators, the formation of a standing wave is most often due to reflection of the wave from the boundaries of the medium or discontinuities impedance. The boundary conditions determine the allowed wavelengths, leading to discrete resonant mods.

In technical analysis, a standing wave is described, among other things, by the standing wave coefficient (VSWR), which reports on the effectiveness of impedance matching in high-frequency systems. The presence of a strong standing wave can lead to energy loss, signal distortion and local system overheating. On the other hand, the conscious use of standing waves in resonant systems enables precise frequency tuning, signal filtering and amplification of oscillations in specific bands.

Transfer Multisort Elektronik (TME) is one of the world’s largest global distributors of electronic components, electrotechnical parts, workshop equipment, and industrial automation. The catalog includes over 1,500,000 products from 1,300 leading manufacturers. TME’s modern logistics centers in Łódź and Rzgów (Poland), with a combined area of over 40,000 m², ship nearly 6,000 packages daily to customers in more than 150 countries.

TME also invests in the development of knowledge and skills of young engineers and electronics enthusiasts through the TME Education project, and supports the tech community by organizing the TechMasterEvent series, promoting innovation and experience exchange.

READ ALSO