+1 500 000 products in offer
7000 packages per day
+300 000 clients from 150 countries
Firmware (firmware) is a specialised type of software embedded in the non-volatile memory of an electronic device that acts as an intermediate between the hardware and the higher layers of an operating or application system. It is integral to the operation of the hardware because it contains the set of instructions and algorithms necessary for its basic operation, configuration and control of operational functions. Unlike typical application software, firmware is directly tied to a specific hardware architecture.
Typically, firmware is stored in non-volatile memory, such as ROM, EEPROM or Flash, which allows it to be retained after power-off. In modern devices, it is becoming increasingly common to update it, e.g. via communication buses or USB Interfaces, allowing bugs to be corrected, features to be added or system security to be enhanced without physical intervention.
Firmware plays a key role in microcontrollers, embedded systems, peripherals (printers, keypads, routers), disk drives, communication interfaces and consumer equipment such as TVs, cameras or audio systems. In many cases, firmware runs first when power is applied, performing initialisation and test routines (e.g. POST in computers) and running further system components.
A characteristic feature of firmware is its deterministic nature and independence from external operating systems, which ensures predictable operation and low latency in device responses. At the same time, it must be designed taking into account resource constraints - such as computing power, memory or power consumption - which requires strict code optimisation and low-level knowledge of the hardware architecture. In terms of security, firmware is also a potential attack vector, so its integrity and ability to be securely updated are important design considerations.
Transfer Multisort Elektronik (TME) is one of the world’s largest global distributors of electronic components, electrotechnical parts, workshop equipment, and industrial automation. The catalog includes over 1,500,000 products from 1,300 leading manufacturers. TME’s modern logistics centers in Łódź and Rzgów (Poland), with a combined area of over 40,000 m², ship nearly 6,000 packages daily to customers in more than 150 countries.
TME also invests in the development of knowledge and skills of young engineers and electronics enthusiasts through the TME Education project, and supports the tech community by organizing the TechMasterEvent series, promoting innovation and experience exchange.