+1 500 000 products in offer

7000 packages per day

+300 000 clients from 150 countries

Quick Buy Favourites
Cart

Photoelasticity - definition

Photoelasticity is the physical phenomenon whereby certain dielectric materials - especially transparent solids such as glass, polycarbonates or epoxies - exhibit a variation in refractive index in response to applied stresses mechanical stresses. When subjected to internal stresses, the material becomes birefringent, meaning that it splits polarised light into two rays with different propagation velocities, depending on the direction and value of the stresses.

This phenomenon is used in an experimental technique called photoelasticity (or photoelastic method), which allows the visualisation and analysis of stress distributions in structural models. It is measured by observing the interference of polarised light passing through a stressed model placed between crossed polarisation filters. The observed isochromes (lines of equal difference in principal stresses) and isopachs (lines of equal sum of stresses) form an interference pattern that can be quantitatively analysed to determine the intensity and orientation of the stresses.

Photoelasticity is used in solid mechanics, materials engineering, biomechanics and in the design of high-reliability components where it is important to know the local stress concentrations. It is non-destructive and highly sensitive, making it useful for both basic research, quality control or verification of numerical models FEA (finite element method). The characteristic parameter for a given photoelastic material is the photoelastic constant, expressing the relationship between the difference in principal stresses and the observed phase difference of light rays.

Transfer Multisort Elektronik (TME) is one of the world’s largest global distributors of electronic components, electrotechnical parts, workshop equipment, and industrial automation. The catalog includes over 1,500,000 products from 1,300 leading manufacturers. TME’s modern logistics centers in Łódź and Rzgów (Poland), with a combined area of over 40,000 m², ship nearly 6,000 packages daily to customers in more than 150 countries.

TME also invests in the development of knowledge and skills of young engineers and electronics enthusiasts through the TME Education project, and supports the tech community by organizing the TechMasterEvent series, promoting innovation and experience exchange.

READ ALSO