+1 500 000 products in offer

7000 packages per day

+300 000 clients from 150 countries

Quick Buy Favourites
Cart

Photoresistors - definition

A Photoresistor (also known as a Light Dependent Resistor, LDR - Light Dependent Resistor) is an electronic component whose resistance varies with the intensity of the light falling on it. In the dark, its resistance is very high (even on the order of megohms), whereas as the light increases, the resistance decreases, often to several hundred ohms (Ω). This phenomenon is due to the photoconductivity effect - in a semiconducting active material (usually cadmium sulphide, CdS), light generates additional charge carriers, increasing the conductivity.

Photoresistors are passive elements with no internal voltage or current source. They do not exhibit polarisation, which means that they can be incorporated into a circuit at will, without regard to the direction of current flow. Their operation depends mainly on the wavelength of the light and the ambient temperature, which affects their sensitivity and response time. Photoresistors' response to changes in illumination is not instantaneous - it is characterised by a certain delay (rise time and fall time), which is why they are not suitable for detecting fast pulses of light.

Photoresistors are used in light sensors, automatic lighting control systems, electronic devices that respond to changes in brightness, and simple alarm or measurement systems due to their simplicity of operation, low price and ease of integration into analogue circuits. However, due to the use of cadmium-containing compounds, their use may be restricted by hazardous substances legislation (e.g. the RoHS directive).

Photoresistors

Transfer Multisort Elektronik (TME) is one of the world’s largest global distributors of electronic components, electrotechnical parts, workshop equipment, and industrial automation. The catalog includes over 1,500,000 products from 1,300 leading manufacturers. TME’s modern logistics centers in Łódź and Rzgów (Poland), with a combined area of over 40,000 m², ship nearly 6,000 packages daily to customers in more than 150 countries.

TME also invests in the development of knowledge and skills of young engineers and electronics enthusiasts through the TME Education project, and supports the tech community by organizing the TechMasterEvent series, promoting innovation and experience exchange.

READ ALSO