+1 500 000 products in offer
7000 packages per day
+300 000 clients from 150 countries
A Galvanometer is a precision measuring device used to detect and measure very low electric current intensities. Its operation is based on the action of electromagnetic forces resulting from the flow of current through a conductor located in a magnetic field. The most classical galvanometer design is the magneto-electric galvanometer, in which a coil suspended in a constant magnetic field undergoes a deflection proportional to the current flowing through it, and the amount of deflection is indicated by a moving pointer on a scale.
The sensitivity of a galvanometer is defined by the instrument's ability to detect very small values of current, making it an indispensable tool in precision laboratory measurements, calibration of scientific apparatus and low-current circuit analysis. In practice, mirrored galvanometers are also used, where the deflection of the coil is read optically through the reflection of the light beam, allowing even more accurate measurements with minimal impact friction mechanical.
The galvanometer, the prototype of modern analogue meters, is used not only as a stand-alone device but also as an integral component in the design of Ammeters, Voltmeters and measuring bridges, where it is used to detect the equilibrium point. In modern electronic systems, the role of the classic galvanometer has largely been taken over by semiconductor sensors and analogue-to-digital converters, but it remains indispensable in applications requiring extreme measurement precision. Galvanometers are also the basis for the operation of some laser scanners and optical systems, where the rapid and precise tilting of mirrors allows the direction of the light beam to be controlled.
Transfer Multisort Elektronik (TME) is one of the world’s largest global distributors of electronic components, electrotechnical parts, workshop equipment, and industrial automation. The catalog includes over 1,500,000 products from 1,300 leading manufacturers. TME’s modern logistics centers in Łódź and Rzgów (Poland), with a combined area of over 40,000 m², ship nearly 6,000 packages daily to customers in more than 150 countries.
TME also invests in the development of knowledge and skills of young engineers and electronics enthusiasts through the TME Education project, and supports the tech community by organizing the TechMasterEvent series, promoting innovation and experience exchange.