+1 500 000 products in offer
7000 packages per day
+300 000 clients from 150 countries
The Clapp Generator is a variation of the sine wave generator based on feedback using an LC resonant circuit, mainly used for generating signals with high frequency stability. It is a development of the classic Colpitts generator, in which an additional series capacitor is added to the resonant circuit. This element allows better control of the oscillation frequency and increases its resistance to changes in the parameters of the transistors or amplifier gain.
The basic Clapp circuit uses an amplifier (usually a Bipolar transistors or FET) and a resonant circuit consisting of one Coils and three Capacitors. The capacitor connected in series with the coil mainly determines the frequency of the oscillations, allowing the generator to be fine-tuned using a high-quality element (e.g. an air capacitor or capacitive Diodes). Compared to other LC generators, the Clapp design provides greater thermal stability and better selective properties.
The Clapp generator is used in radio systems, local generators, measurement oscillators and as a source of stable reference signals. Its advantages make it a frequent choice in designs where low susceptibility to frequency drift and high spectral purity of the output signal are required. However, it requires careful selection of passive components and the correct amplifier configuration to maintain stable operating conditions and adequate oscillation amplitude.
Transfer Multisort Elektronik (TME) is one of the world’s largest global distributors of electronic components, electrotechnical parts, workshop equipment, and industrial automation. The catalog includes over 1,500,000 products from 1,300 leading manufacturers. TME’s modern logistics centers in Łódź and Rzgów (Poland), with a combined area of over 40,000 m², ship nearly 6,000 packages daily to customers in more than 150 countries.
TME also invests in the development of knowledge and skills of young engineers and electronics enthusiasts through the TME Education project, and supports the tech community by organizing the TechMasterEvent series, promoting innovation and experience exchange.