+1 500 000 products in offer

7000 packages per day

+300 000 clients from 150 countries

Quick Buy Favourites
Cart

Gambling - definition

Hazard in digital systems is the phenomenon of an undesired, short-term change in the logic state of the output signal that occurs despite constant or predictable values of the input signals. It arises as a result of differences in propagation times of signals in different logic paths, leading to a temporary inconsistency in the logic state that can interfere with system operation. Hazards are particularly important in combinational circuits, counters, registers and any system that operates synchronously, where even a short pulse can affect incorrect state switching.

The occurrence of gambles is a consequence of the physical properties of real logic gates, which - unlike ideal models - do not change state immediately, but with a delay that depends on their design and load. Variations in these delays can lead to a situation where the output of the circuit takes on the wrong logic value for a fraction of a microsecond, even though the state of the inputs theoretically should not cause this.

Hazards can be classified as static, dynamic and functional, among others, depending on the nature of the erroneous signal and the context in which it occurs. In practice, their presence makes it difficult to design reliable digital systems, especially in high-frequency circuits or where signals are passed on to components sensitive to interference pulses.

Appropriate design techniques such as signal synchronisation, insertion of additional delays, timing-error-tolerant design or the use of sequential circuits with precisely controlled clock waveforms are used to minimise the risk of gambles. Verifying the presence of gambles is an important timing analysis step in digital circuit design and is often supported by simulation tools.

Transfer Multisort Elektronik (TME) is one of the world’s largest global distributors of electronic components, electrotechnical parts, workshop equipment, and industrial automation. The catalog includes over 1,500,000 products from 1,300 leading manufacturers. TME’s modern logistics centers in Łódź and Rzgów (Poland), with a combined area of over 40,000 m², ship nearly 6,000 packages daily to customers in more than 150 countries.

TME also invests in the development of knowledge and skills of young engineers and electronics enthusiasts through the TME Education project, and supports the tech community by organizing the TechMasterEvent series, promoting innovation and experience exchange.

READ ALSO