+1 500 000 products in offer

7000 packages per day

+300 000 clients from 150 countries

Quick Buy Favourites
Cart

Geiger counter - definition

The Geiger Counter is a detector of ionising radiation, used to record alpha particles, beta particles and gamma radiation. Its operation is based on the phenomenon of gas ionisation in a sealed tube, called a Geiger-Müller tube, which acts as a detection chamber. The inside of the tube is filled with a mixture of inert gases at the appropriate pressure, and a high voltage, close to the breakthrough threshold, is maintained between the central anode and the surrounding cathode.

When a radiation particle enters the detector, it ionises the gas molecules, triggering a cascading electron avalanche. The resulting electrical pulse is short but distinct and can be easily counted by the electronics. Each recorded particle causes a single pulse, regardless of its energy, so that the Geiger counter does not provide information about the intensity of the radiation, but only about its presence and frequency of events.

This device has found wide application in radioactive contamination detection, environmental control, nuclear physics and safety in working with radioactive materials. Its structural simplicity, high sensitivity and ability to detect different types of radiation make it a useful Measuring Tools, especially in field conditions. To increase the selectivity of the measurements, additional Guards and filters are used to reduce the impact of certain types of particles.

The Geiger counter requires periodic resetting after each pulse due to the so-called dead time, i.e. the period during which the system is not capable of recording another event. To prevent continuous discharges, quenching compounds are added to the gas to reduce the number of secondary ionisations. Modern versions of counters are equipped with digital circuits that allow real-time recording, analysis and presentation of measurement data.

Transfer Multisort Elektronik (TME) is one of the world’s largest global distributors of electronic components, electrotechnical parts, workshop equipment, and industrial automation. The catalog includes over 1,500,000 products from 1,300 leading manufacturers. TME’s modern logistics centers in Łódź and Rzgów (Poland), with a combined area of over 40,000 m², ship nearly 6,000 packages daily to customers in more than 150 countries.

TME also invests in the development of knowledge and skills of young engineers and electronics enthusiasts through the TME Education project, and supports the tech community by organizing the TechMasterEvent series, promoting innovation and experience exchange.

READ ALSO