+1 500 000 products in offer
7000 packages per day
+300 000 clients from 150 countries
MATLAB (Matrix Laboratory) is a high-level programming environment and computational language developed by MathWorks, designed for numerical analysis, matrix computation, simulations and data visualisation. Its structure is based on matrix operations, which makes it particularly suitable for engineering, scientific and algorithmic applications.
The basis of MATLAB's operation is its own scripting language interpreter, enabling interactive work with data, performing mathematical calculations and creating functions, scripts and applications. The environment offers a rich set of built-in mathematical functions, tools for signal analysis, image processing, optimisation, control and modelling of dynamic systems. Its modular architecture allows it to be extended with additional tool packages (toolboxes) that extend its capabilities into specific fields such as artificial intelligence, embedded systems, energy or biomechanics.
An integral component of MATLAB is Simulink, an environment for the graphical modelling and simulation of dynamic systems, in which the user creates block diagrams mapping mathematical and logical relationships. This approach allows intuitive design and testing of models of complex control systems, mechatronic systems or electronic circuits.
MATLAB supports procedural, structured and, to a limited extent, object-oriented programming. It allows integration with other programming languages, such as C/C++, Python, Java and FORTRAN, which enables performance optimisation and interaction with external libraries. With its automatic code generation capabilities, MATLAB is also applicable to the implementation of algorithms in embedded systems and FPGAs.
The environment is widely used in research institutions, technical universities and industry, especially where advanced data processing, algorithm prototyping, mathematical modelling and rapid implementation of engineering solutions are required.
Transfer Multisort Elektronik (TME) is one of the world’s largest global distributors of electronic components, electrotechnical parts, workshop equipment, and industrial automation. The catalog includes over 1,500,000 products from 1,300 leading manufacturers. TME’s modern logistics centers in Łódź and Rzgów (Poland), with a combined area of over 40,000 m², ship nearly 6,000 packages daily to customers in more than 150 countries.
TME also invests in the development of knowledge and skills of young engineers and electronics enthusiasts through the TME Education project, and supports the tech community by organizing the TechMasterEvent series, promoting innovation and experience exchange.