+1 500 000 products in offer

7000 packages per day

+300 000 clients from 150 countries

Quick Buy Favourites
Cart

Niuton (N) - definition

The Niuton (N) is the unit of force measurement in the UoM (International System of Units), defined as the force that gives a body with a mass of one kilogram an acceleration of one metre per second squared (1 N = 1 kg-m/s²). The unit is named after Sir Isaac Newton, whose second principle of dynamics, formulated in the 17th century, defines the fundamental relationship between force, mass and acceleration.

In physical terms, the newton describes the action of a cause that changes the motion of a body - both its speed and direction. The force expressed in newtons is a vector quantity, having both a value and a direction of action, which is crucial in the analysis of mechanical phenomena such as equilibrium, uniformly varying motion or dynamic interactions.

In engineering and technical practice, the newton is the basic unit used to define forces in building structures, machinery, mechanical devices and propulsion systems. In fields such as solid mechanics, aerodynamics, robotics and biomechanics, the analysis of force values expressed in newtons allows the design of safe and efficient technical systems.

For forces used in more precise contexts or those requiring high sensitivity, such as micro- and nanoscale measurements, multiples or aliquots of the newton unit, such as micronutons (μN) or kilonutons (kN), are used to adapt the measurement range to the specific application. In complex systems, the analysis of force and moment distributions, also expressed in newtons and newton-metres (N-m), is fundamental in strength testing and dynamics of mechanical systems.

Transfer Multisort Elektronik (TME) is one of the world’s largest global distributors of electronic components, electrotechnical parts, workshop equipment, and industrial automation. The catalog includes over 1,500,000 products from 1,300 leading manufacturers. TME’s modern logistics centers in Łódź and Rzgów (Poland), with a combined area of over 40,000 m², ship nearly 6,000 packages daily to customers in more than 150 countries.

TME also invests in the development of knowledge and skills of young engineers and electronics enthusiasts through the TME Education project, and supports the tech community by organizing the TechMasterEvent series, promoting innovation and experience exchange.

READ ALSO