+1 500 000 products in offer

7000 packages per day

+300 000 clients from 150 countries

Quick Buy Favourites
Cart

Voltage transformer - definition

The voltage transformer is an electromagnetic device used in the electric power industry for the proportional conversion of the high voltage in the power grid to a lower voltage that is safe for measurement, protection and control systems. Its main function is to provide galvanic isolation between the high voltage circuits and the low voltage secondary circuits, while allowing the primary voltage value to be accurately represented on a reduced scale.

The operation of a voltage transformer is based on the principle of voltage transformation in the ferromagnetic core, just as in a classical transformer. The mains voltage flows in the primary winding, while a proportional voltage is induced in the secondary winding, according to the established transformer. Typical secondary voltages are standardised, most often 100 V or 110 V, which facilitates integration with measuring devices and protection relays.

Depending on the application, voltage transformers can be manufactured as dry, oil, gas (SF₆) or capacitive, especially for very high voltages. The design and parameters of these devices must ensure high voltage reproduction accuracy and resistance to disturbances and overloads. The accuracy classes of the transformers are defined in standards and their selection depends on the requirements of the specific application, e.g. whether it is a precise measurement or only the detection of fault conditions.

Due to its functions, the voltage transformer is an indispensable component of power protection and automation systems, enabling safe voltage monitoring in transmission and distribution networks, both in high-voltage substations and in industrial installations.

Voltmeters for use with a voltage transformer

Transfer Multisort Elektronik (TME) is one of the world’s largest global distributors of electronic components, electrotechnical parts, workshop equipment, and industrial automation. The catalog includes over 1,500,000 products from 1,300 leading manufacturers. TME’s modern logistics centers in Łódź and Rzgów (Poland), with a combined area of over 40,000 m², ship nearly 6,000 packages daily to customers in more than 150 countries.

TME also invests in the development of knowledge and skills of young engineers and electronics enthusiasts through the TME Education project, and supports the tech community by organizing the TechMasterEvent series, promoting innovation and experience exchange.

READ ALSO