+1 500 000 products in offer
7000 packages per day
+300 000 clients from 150 countries
A digital-to-analog converter (DAC, or digital-to-analog converter) is an electronic circuit used to convert a digital signal, represented by a sequence of numerical values, into a corresponding analogue signal of continuous amplitude. The DAC plays a key role in systems where post-digital processing data must be presented in analogue form - for example, for controlling actuators, generating sound or video representation of information.
The operation of the converter is based on the inverse of the process carried out by an analogue-to-digital converter (ADC). Each digital value, usually stored in binary form, is converted into a corresponding voltage or current level, according to a fixed conversion range and resolution. The result is a stepped signal, which can then be smoothed using analogue filters to produce a waveform with smooth variations.
The key parameters of a DAC are resolution (number of bits), accuracy, processing speed and output voltage range. The higher the resolution, the more output levels can be generated, resulting in smaller differences between successive signal values and a more detailed representation of the digital signal. The processing speed determines how often the converter can update the state of the output, which is important in applications that require analogue values to change dynamically.
DACs are used in audio systems, industrial automation, Measuring Instruments, musical instruments, control systems, and systems that generate modulated signals. Others architectures are used depending on the application, such as resistive-weighted, ladder R-2R, sigma-delta or pulse-width modulated converters. The choice of the appropriate technology depends on the requirements for precision, speed and noise level.
Transfer Multisort Elektronik (TME) is one of the world’s largest global distributors of electronic components, electrotechnical parts, workshop equipment, and industrial automation. The catalog includes over 1,500,000 products from 1,300 leading manufacturers. TME’s modern logistics centers in Łódź and Rzgów (Poland), with a combined area of over 40,000 m², ship nearly 6,000 packages daily to customers in more than 150 countries.
TME also invests in the development of knowledge and skills of young engineers and electronics enthusiasts through the TME Education project, and supports the tech community by organizing the TechMasterEvent series, promoting innovation and experience exchange.