+1 500 000 products in offer

7000 packages per day

+300 000 clients from 150 countries

Quick Buy Favourites
Cart

Thermal resistance - definition

Thermal resistance is a physical quantity that describes the resistance that a material or system gives to the flow of heat. It is analogous to electrical resistance, but refers to thermal conductivity rather than electrical conductivity. In its simplest terms, it defines what temperature difference is needed for a unit heat flux to flow through an element. The unit of thermal resistance in SI is kelvin per watt (K/W).

In a technical context, thermal resistance occurs in the description of heat flow through homogeneous and complex structures - from single layers of materials to entire electronic systems. It is defined as the ratio of the temperature difference between two points to the heat power flowing between them. In real systems, it can take into account both thermal conductivity in solids and the resistance associated with conduction across contact surfaces, convection or radiation.

Thermal resistance is of particular importance in electronics and electrical engineering, where it enables an assessment of the ability of components to dissipate heat generated during operation. This parameter is crucial in the design of power circuits, power transistors, Power LEDs, microprocessors and devices requiring cooling. An established thermal resistance limit allows an assessment of whether a component will operate within a safe temperature range or whether it requires a heat sink, heat conductive compounds or other cooling systems.

In complex structures, the thermal resistance can be a series sum of the resistances of the individual material layers and contacts. The variation of this parameter as a function of temperature, contact surface, roughness, mechanical pressure and physicochemical properties of the surface is also taken into account. Accurate modelling and control of thermal resistance is an important part of thermal engineering, with implications for the reliability and performance of technical systems.

Transfer Multisort Elektronik (TME) is one of the world’s largest global distributors of electronic components, electrotechnical parts, workshop equipment, and industrial automation. The catalog includes over 1,500,000 products from 1,300 leading manufacturers. TME’s modern logistics centers in Łódź and Rzgów (Poland), with a combined area of over 40,000 m², ship nearly 6,000 packages daily to customers in more than 150 countries.

TME also invests in the development of knowledge and skills of young engineers and electronics enthusiasts through the TME Education project, and supports the tech community by organizing the TechMasterEvent series, promoting innovation and experience exchange.

READ ALSO