+1 500 000 products in offer

7000 packages per day

+300 000 clients from 150 countries

Quick Buy Favourites
Cart

Shoal robotics - definition

Shoal robotics (swarm robotics) is a field of robotics inspired by phenomena of collective behaviour found in nature, such as the movements of schools of fish, swarms of insects or flocks of birds. It focuses on the design, modelling and control of groups of simple, relatively small robots that work together in a decentralised manner to perform complex tasks without an overarching controller. Such a system is characterised by high scalability, robustness to unit failure and adaptability in dynamic environments.

Each robot in the shoal operates on the basis of local information obtained from the environment or from communication with the nearest units. Their behaviour is determined by simple rules that, when combined, lead to the emergence of complex global patterns of action. Central to shoal robotics is the autonomy of individual agents, limited perception of the environment, asynchronous operation and lack of centralised coordination.

Technologies being developed within this field are finding applications in space exploration, environmental monitoring, rescue operations, precision agriculture, storage and transportation, as well as military applications and scientific research, among others. Thanks to their distributed structure, these systems can continue to operate even when some units fail, and their numbers can be flexibly increased without changing the control algorithms.

Shoal robotics uses Tools from bio-inspired algorithms, control theory, machine learning and multi-agent systems. It also requires the development of effective methods of communication, collision avoidance, relative localisation and consensus, which are essential to achieve coordination and cooperation between units in a dynamic environment.

Robotics and Prototyping

Transfer Multisort Elektronik (TME) is one of the world’s largest global distributors of electronic components, electrotechnical parts, workshop equipment, and industrial automation. The catalog includes over 1,500,000 products from 1,300 leading manufacturers. TME’s modern logistics centers in Łódź and Rzgów (Poland), with a combined area of over 40,000 m², ship nearly 6,000 packages daily to customers in more than 150 countries.

TME also invests in the development of knowledge and skills of young engineers and electronics enthusiasts through the TME Education project, and supports the tech community by organizing the TechMasterEvent series, promoting innovation and experience exchange.

READ ALSO