+1 500 000 products in offer

7000 packages per day

+300 000 clients from 150 countries

Quick Buy Favourites
Cart

Electrical switchgear - definition

Electrical switchgear is an assembly of electrical power equipment used to distribute, control, protect and measure electricity in low, medium or high voltage systems. It is a key component of the power infrastructure, providing a safe and orderly connection between power sources and energy consumers. Switchgear comes in a variety of configurations and scales, from simple domestic installations to complex industrial systems and transmission networks.

Structurally, the switchgear consists of a protective enclosure and switchgear, protection, measurement and control equipment mounted inside, such as circuit breakers, disconnectors, contactors, fuses, transformers or relays. These components are installed in such a way as to allow easy service access and to ensure adequate conditions for cooling, protection against electric shock and thermal overload.

Switchgear is divided into substation, main, branch and terminal, depending on where it is used in the structure of the power system. They can be free-standing, recessed, modular or prefabricated, and their design must comply with the applicable technical standards, e.g. EN 61439. Important parameters are degree of protection IP, short-circuit resistance, rated current and rated voltage.

The functionality of switchgear includes not only energy flow management, but also rapid shutdown of circuits in the event of a fault, protecting people and equipment from the effects of short circuits, overloads and surges. In modern installations, switchgear is integrated with building automation, condition monitoring and remote energy management systems. Proper selection and configuration of the switchgear is crucial to the reliability, efficiency and safety of the entire power system.

Transfer Multisort Elektronik (TME) is one of the world’s largest global distributors of electronic components, electrotechnical parts, workshop equipment, and industrial automation. The catalog includes over 1,500,000 products from 1,300 leading manufacturers. TME’s modern logistics centers in Łódź and Rzgów (Poland), with a combined area of over 40,000 m², ship nearly 6,000 packages daily to customers in more than 150 countries.

TME also invests in the development of knowledge and skills of young engineers and electronics enthusiasts through the TME Education project, and supports the tech community by organizing the TechMasterEvent series, promoting innovation and experience exchange.

READ ALSO