+1 500 000 products in offer

7000 packages per day

+300 000 clients from 150 countries

Quick Buy Favourites
Cart

Seismograph - definition

The seismograph is a specialised measuring device for the detection, recording and analysis of seismic waves generated by natural or artificial vibrations of the earth's crust. It works on the principle of measuring the relative displacement of an inert mass with respect to the Enclosures of the device, which makes it possible to map the mechanical characteristics of the propagating waves. The structural foundation of a classical seismograph is an oscillating mechanical system with a mass suspended on an elastic element, whose inertia allows ground motions to be mapped as a function of time. Modern seismographs use electromechanical, optoelectronic or MEMS solutions, enabling high sensitivity and resolution over a wide frequency range.

Seismic signals are recorded in the form of seismograms, which allow the identification of parameters such as amplitude, frequency, P- and S-wave arrival time and vibration energy. Interpretation of these data makes it possible to locate the epicentre, determine the depth of the focus and estimate the magnitude of the earthquake. Seismographs can operate in one-dimensional systems (recording one component of motion) or triaxial systems, analysing the full vector structure of vibrations. Their applications range from monitoring tectonic activity to assessing the stability of engineering structures or analysing anthropogenic vibrations in urbanised environments.

Transfer Multisort Elektronik (TME) is one of the world’s largest global distributors of electronic components, electrotechnical parts, workshop equipment, and industrial automation. The catalog includes over 1,500,000 products from 1,300 leading manufacturers. TME’s modern logistics centers in Łódź and Rzgów (Poland), with a combined area of over 40,000 m², ship nearly 6,000 packages daily to customers in more than 150 countries.

TME also invests in the development of knowledge and skills of young engineers and electronics enthusiasts through the TME Education project, and supports the tech community by organizing the TechMasterEvent series, promoting innovation and experience exchange.

READ ALSO