+1 500 000 products in offer
7000 packages per day
+300 000 clients from 150 countries
Charging station (Electric Vehicle Supply Equipment (EVSE) is an infrastructural technical system for the transmission of electrical energy from the mains supply to electric vehicle (EV) traction batteries. This device acts as an intermediary between the energy source and the vehicle's charging management system, carrying out the energy transmission process in a safe, controlled manner and in compliance with current communication standards and data transmission protocols.
Others can operate in different power supply modes, either using alternating current (AC) - for slow and semi-fast charging stations - or direct current (DC), specific to fast charging installations. Built-in protection systems, such as RCD Circuit Breakers, vehicle presence detection systems, ground integrity monitoring systems and communication functions (e.g. ISO 15118 compliance), provide both operational safety and dynamic energy management capabilities in the context of smart grids.
Modern charging stations can be equipped with wireless communication modules, access authorisation systems, HMI interfaces and energy consumption monitoring functions. They require compliance with IEC, SAE, GB/T or CHAdeMO standards, depending on the region and vehicle technology. They play a key role in the development of electromobility and are an important part of the energy transition and decarbonisation of transport.
Transfer Multisort Elektronik (TME) is one of the world’s largest global distributors of electronic components, electrotechnical parts, workshop equipment, and industrial automation. The catalog includes over 1,500,000 products from 1,300 leading manufacturers. TME’s modern logistics centers in Łódź and Rzgów (Poland), with a combined area of over 40,000 m², ship nearly 6,000 packages daily to customers in more than 150 countries.
TME also invests in the development of knowledge and skills of young engineers and electronics enthusiasts through the TME Education project, and supports the tech community by organizing the TechMasterEvent series, promoting innovation and experience exchange.