+1 500 000 products in offer

7000 packages per day

+300 000 clients from 150 countries

Quick Buy Favourites
Cart

Symmetrizer (balun) - definition

The symmetrizer, also known as balun (short for balanced-unbalanced), is an electronic device used to transform signals between symmetrical and asymmetrical lines. Its purpose is to ensure correct impedance matching and to minimise unwanted signal interference resulting from differences in the structure of the transmission paths.

In a symmetrical line, such as twisted-pair or symmetrical dipole, the signal is transmitted via two cables with equal parameters with respect to earth, which ensures high resistance to electromagnetic interference. In contrast, an asymmetrical line, such as a coaxial cable, transmits the signal via a single wire relative to a common ground. Without a suitable transformation, potential differences can arise when such lines are connected, leading to noise emissions, signal losses or common ground currents.

Baluns can be implemented in a variety of ways, depending on frequency and signal characteristics: as electromagnetic transformers, capacitive systems, or hybrid designs based on cores Ferrite Cores. In radiocommunication, television, radar systems and RFID technologies symmetisers play a key role in ensuring high quality signal transmission by eliminating asymmetry and suppressing interference from external sources.

In the context of antenna design, baluns are an indispensable design element, which enables proper adaptation between symmetrical antennas and asymmetrical transceiver systems, directly influencing radiation efficiency, impedance matching and limiting the emission of unwanted waves in the transmission path. A properly selected symmetriser not only improves the performance of an RF system, but also significantly affects its reliability and compliance with electromagnetic compatibility (EMC) standards.

Transfer Multisort Elektronik (TME) is one of the world’s largest global distributors of electronic components, electrotechnical parts, workshop equipment, and industrial automation. The catalog includes over 1,500,000 products from 1,300 leading manufacturers. TME’s modern logistics centers in Łódź and Rzgów (Poland), with a combined area of over 40,000 m², ship nearly 6,000 packages daily to customers in more than 150 countries.

TME also invests in the development of knowledge and skills of young engineers and electronics enthusiasts through the TME Education project, and supports the tech community by organizing the TechMasterEvent series, promoting innovation and experience exchange.

READ ALSO